Electrolytic Decoupling Capacitors - 10uF/25V

Low-profile electrolytic decoupling capacitors 10uF/25V. These capacitors are great transient/surge suppressors and work well as charge pump caps for MAX232 circuits. High quality radial electrolytic capacitors.

Check out our Unregulated Power Supply Tutorial

Electrolytic Decoupling Capacitors - 10uF/25V Product Help and Resources

Sound Detector Hookup Guide

February 27, 2014

The Sound Detector is a microphone with a binary output. This guide explains how it works and how you can use it in your projects.

Capacitors

June 19, 2013

Learn about all things capacitors. How they're made. How they work. How they look. Types of capacitors. Series/parallel capacitors. Capacitor applications.

Proto Pedal Example: Programmable Digital Pedal

September 22, 2016

Building a pedal around the Teensy 3.2 and Teensy Audio shield. Changing the effect in the pedal is as easy as uploading a new sketch!

Core Skill: Soldering

This skill defines how difficult the soldering is on a particular product. It might be a couple simple solder joints, or require special reflow tools.

2 Soldering

Skill Level: Rookie - The number of pins increases, and you will have to determine polarity of components and some of the components might be a bit trickier or close together. You might need solder wick or flux.
See all skill levels


Core Skill: Electrical Prototyping

If it requires power, you need to know how much, what all the pins do, and how to hook it up. You may need to reference datasheets, schematics, and know the ins and outs of electronics.

3 Electrical Prototyping

Skill Level: Competent - You will be required to reference a datasheet or schematic to know how to use a component. Your knowledge of a datasheet will only require basic features like power requirements, pinouts, or communications type. Also, you may need a power supply that?s greater than 12V or more than 1A worth of current.
See all skill levels


Comments

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • At least we know SparkFun isn't cheap if they are telling you, you can get these cheaper from such and such. that only makes me want to get it from Sparkfun because of the honesty.

    • Jabrwock / about 10 years ago / 2

      It's a shipping vs price tradeoff. Sparkfun charges less than Digikey for shipping, but Digikey charges less per unit, with greater discounts the more you order.

      Right now they even out at about 20 pcs. So if you need less, go with Sparkfun.

    • Member #139441 / about 11 years ago / 1

      It should not really be all that surprising, Digikey is a hell of a lot bigger than Sparkfun.

    • The Doctor Doge / about 11 years ago / 1

      If you only want one, I go with sparkfun

  • PickledDog / about 9 years ago / 1

    It's worth noting that these don't look like the picture any more. They're much nicer now :)

    These the the 'stubby' type, as seen in the SparkPunk Sound Kit and RedBoard PTH. Much more handy and compact.

  • Parizival / about 10 years ago / 1

    Do these still work as a regular 10uF capacitor?

    • PointyOintment / about 9 years ago / 1

      As far as I can tell, they are regular capacitors, so yes.

Customer Reviews

No reviews yet.