Search
Baby Bluetoothby Nate |
August 3, 2009 |
|
The final class of the SparkFun summer semester is tonight! Come join us for a class on selling your widget!

I'm not sure if you've seen these little jobbers on the market. It's an itty-bitty Bluetooth dongle meant for laptops. Above, you can see the small nub sticking out of the side of my HP Mini 1000, which absolutely rocks, but does not have Bluetooth built in.
Depending on where you buy, these little guys range from a few dollars to $50! But what is the world could be tightly packed underneath that little cover?

Depending on where you buy, these little guys range from a few dollars to $50! But what is the world could be tightly packed underneath that little cover?

They must have folded the PCB, stacked the dies, used a mechanical turk inside or managed some sort of magic. That's just amazing!


I figured the entire thing would have been one potted glob of black resin, but with a handy razor blade, the housing split open surprisingly easily. That is one heck of a PCB trace antenna (2.4GHz).
The engineering was surprisingly good! The PCB slides inside the small metal housing, that acts as the USB connector and doubles as an RF shield. Very sneaky. Here you can see the 12MHz crystal (for USB communication) and a simple 3-pin SMT voltage regulator (I assume 5V down to 3.3V). There is also a basic LED on this side of the PCB that barely lights up and can be seen through the smoky, semi-transparent housing.
The engineering was surprisingly good! The PCB slides inside the small metal housing, that acts as the USB connector and doubles as an RF shield. Very sneaky. Here you can see the 12MHz crystal (for USB communication) and a simple 3-pin SMT voltage regulator (I assume 5V down to 3.3V). There is also a basic LED on this side of the PCB that barely lights up and can be seen through the smoky, semi-transparent housing.
Comments
21 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.







http://www.engadget.com/2009/01/15/buffalos-802-11n-wifi-dongle-small-in-size-tiny-in-price/
Importantly, it works with Linux. Annoyingly, the light flashes whenever it has power, which includes when I have shutdown my computer. So I have to pull it out whenever I go to bed.
I've notice a disturbing trend among devices - gratuitously bright LEDs. The blue ones are the worst. The blinking blue one on the wireless fob for Wii rockband is so fricking bright that you can read by it with the lights off and it continually distracts when watching the tube. I had to hack it. And the USB cell phone charger for my car has one that is so bright it's reflection is distracting at night.
http://www.geekstuff4u.com/buffalo-16gb-5mm-thumbkey.html
Logictech also uses the same package for wireless keyboard/mouse:
http://www.techwithoutwires.com/50226711/logitech_wireless_mouse_with_mini_receiver.php
http://www.dealextreme.com/products.dx/category.304~search.usb%20bluetooth
http://www.dealextreme.com/details.dx/sku.12696
http://www.dealextreme.com/details.dx/sku.11866
Of course if you want LONG range... http://www.aircable.net/host-xr.html
Or small for my embedded (the ESD200 series) - Sparkfun has modules but I think this is smaller and has pins: http://www.sena.com/products/industrial_bluetooth/index.php?tab_menu=ESD
http://www.iogear.com/product/GBU421/
It works perfectly with Windows, Mac, and Linux for communication with the Wiimote using the default OS Bluetooth stack. No crazy Bluetooth drivers needed!
http://gizmodo.com/5329350/logitech-unifying-receiver-pairs-with-multiple-keyboards-and-mice-at-once/gallery/
http://www.akihabaranews.com/en/news_details.php?id=18632
I mean, would it be easy to interface this dongle with a micro controller?
Arduino BT costs U$90. This dongle costs U$5 with free shipping.
Thanks,
Franklin Dattein
the cheapest way to get arduino talking over bluetooth is to use the Blue Smirf module =)
http://www.circuitsathome.com/products-page/arduino-shields/usb-host-shield-for-arduino
(every part connected to usb conector on this board will get 9V)
can the on board SMT voltage regulator will handle 9V, is there any comapny to ask?
thanks