Search
Product Info
Breadboard Power Supply 5V/3.3V
sku: PRT-00114
Description: A very simple breadboard power supply kit that takes power from a DC wall wart and outputs a selectable 5V or 3.3V regulated voltage. The .1" headers are mounted on the bottom of the PCB for simple insertion into a breadboard. Pins labeled VCC and GND plug directly into the power lines. The lone pair of pins have no electrical connection but help support the PCB.
There are two pins available within the barrel jack footprint. Any stripped +/- DC supply can be connected instead of the barrel connector. Board has both an On/Off switch and a voltage select switch (3.3V/5V).
Comes as a bag of parts kit and is easily assembled if you can follow the silkscreen indicators and have beginning experience with a soldering iron. You will need to read the resistor bands or use a multimeter to determine the resistor sizes.
Check out our Unregulated Power Supply Tutorial!
Kit Contains:
- DC Barrel Connector (2.1mm center positive)
- TO-220 Voltage Regulator (LM317 1.5A max current)
- 1N4004 Reverse Protection Diode
- 100uF 25V Capacitor
- 10uF 25V Capacitor
- 0.1uF 50V Capacitor
- Red Power LED - High Brightness
- 2pcs SPDT Slide Switch
- 4pcs 0.1" Header Pins
- 2pcs 330 Resistor 1/6W
- 390 Resistor 1/6W
- 240 Resistor 1/6W
- Bare PCB with Silkscreen Indicators
- PTC resettable fuse
Documents: Schematic
Dimensions: 1.25x1.25"
Pricing
Comments
44 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.






















~thanks!
Is the last one nessesary ?
The free spot on the board reads "PTC"
The max input voltage of the Lm317 is 40 volts but the schematic says it's max 10 volts. Does it get to hot when used with an 15 volt supply or can it be done?
Excellent little kit, really easy to assemble, and a great regulated power supply for projects.
Thanks to the wonderfull silkscreen, the kit could be soldered together in no time and without having to look at the schematic or anything else.
Congratulations on another fine product.
One tip: To make the pins a bit more sturdy, I put a tiny bit of superglue on the underside of the board where they join the board.
I also wish that it was made more clear that the max input was 12V. I now need to scrounge a 50V cap for a 24V input.
I get bypassing the PTC if I want to be able to supply more current (and I've got a TO-220 heat sink kit in the parts box, I'll see if it fits), and doing something to avoid LED eye burnout :-)
The last time I remember looking at the LMx17 datasheet, I thought a 10uF bypass from the adjust pin to ground improved ripple rejection significantly. I don't see anything like that on the schematic. Is that an old technique that isn't necessary with modern LM317s, not done to keep cost and/or size down, or for some other reason?
http://www.flickr.com/photos/sparkfun/3926747868/
Thanks to the comments on here i replaced the super bright led with different one that doesn't blind!.
Good job guys .. this is way fun!
The 100uf cap is to smooth out the bigger ripples before the regulator. Then, the regulator does its best to smooth the electricity flow even more. However, it doesn't do a good job a the higher frequencies of ripple so the smart engineer places to small caps a the Vout side to smooth it out even more. Thats my edgy-cated guess :D.
I then checked the voltages and got 3.34 volts on the 3.3v and 5.12 volts on the 5v. It's all good. Thanks SparkFun for such a good kit. :)
it seems similar to this design http://miskatonic-tech.blogspot.com/2009/12/usb-powered-nintendo-wii-remote-wiimote.html
If you can contact us at techsupport at sparkfun dot com, we will get you all taken care of.
Thanks,
Pearce
Product Suggestion: to complement this breadboard power supply. I would love to have just a small serial 1x8 LCD or as big as 2x16 if not too heavy I'm good with a couple of legs to touch my desk in order to get 2x16, setup like this power supply with the pins lined up for a Breadboard. So instead of using a single LED to debug programs with, I could use that same "Debug" pin to get real information from my programs.