Search
Product Info
AVR STK Serial Port Dongle Programmer
sku: PGM-00014
Description: AVR-PG1B is programmer based on serial port PonyProg design. It takes the power supply from the target board. The connector is 2x5 pin with 0.1" step and Atmel STKxxx compatible layout.
Dimensions: 45x30 mm (1.7x1.2") + 20 cm (8") cable
Documents: avr-pg1b.pdf, AVR-PG1B schematic, AVR ICSP connector
Software: FREE PonyProg from Claudio Lanconelli
Supported Devices: The currently supported devices by PonyProg software, which can be programmed by AVR-PG1B are:
AT90S1200, AT90S2313, AT90S2323, AT90S2343, AT90S4414, AT90S4434, AT90S8515, AT90S8535, AT90S2323, AT90S2343, AT90S2333, AT90S4433, AT90S4434, AT90S8535, AT90S8534, ATmega103, ATmega161, ATmega163, ATmega323, ATmega128, ATmega8, ATmega16, ATmega64, ATtiny12, ATtiny15
Pricing
Comments
11 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.


















And in case you were wondering if it will program your MCU using a 3.3V supply, it does. :-)
-Matt
So, it seems like Serial->USB is working at least to talk to the programmer. OSX Snow Leopard with KeySpan USB Serial adapter. I will update if I get the chip programmed with this setup.
i made it work with both the arduino IDE and avrdude. They both need some tweaking though.
AVRdude: you have to add support for atmega328p in case there isn't. Search for the .CONF file and add this part to it: http://www.tuxgraphics.org/common/src2/article09101/atmega328.html
Arduino IDE: modify the boards.txt file. Either add your own board or modify an existing, but make sure the upload protocol is "ponyser" and not "stk500".
If you need help feel free to mail me at frsmnk at msn dot com.
:)