Search
Product Info
MPLAB Compatible ICD2 with USB and RS232
sku: PGM-00005
Description: The popular ICD2 by Olimex. This is complete drop in replacement for the Microchip ICD2 at a fraction of the cost. A low cost development tool providing real time emulation for all PICs with the built-in ICD feature. Operates through RS232 or USB. More information about the ICD2 can be found on Microchip's web site.Uses standard DB9 serial cable or USB cable. USB cable should be 'B' Male (ICD2) to 'A' Male (Computer).
The large PIC on the ICD2 is a 16F877 that stays on the board. It is what does all the magic. The ICD2 can only be used through the ICSP port - there is no 'programming' socket on the unit itself.
Note: MPLab 8.xx has a bug that affects the RS232 interface on the ICD2. If using version 8.xx of Microchip's MPLab, you will need to use the USB interface or any of the version 7.xx IDEs. This bug affects not only Olimex ICD2s, but the original MPLab ICD2 from Microchip as well.Documents: PIC ICSP connector (top view)
Software: MPLAB-IDE
Dimensions: 3.8x3.3"
Pricing
Comments
4 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.























I also have a PICStart Plus, and I tried to burn a new 16F877A on it to get my original ICD2 functioning, but I still get teh error message when trying to connect :
ICD0021: Unable to connect with MPLAB ICD 2
Where can I get the proper firmware for teh Olimex ?
I would like to keep it as an an emergency spare.
Thanks
http://forum.sparkfun.com/viewtopic.php?t=2239&highlight=icd2+firmware+16f877a
The BL010100.HEX file did NOT do the trick.
I registered and downloaded the one from:
http://www.edaboard.com/viewtopic.php?t=74753&postdays=0&postorder=asc&highlight=icd2&start=0
as mentioned elsewhere in the thread.