Search
Product Info
Breakout Board for FT232RL USB to Serial
sku: BOB-00718
Description: Basic breakout board for FTDI's popular USB to UART IC. Now with internal oscillator and EEPROM, the FT232RL is an impressive IC!
VCCIO is now tied to 3.3V through a solder jumper. You have the option of clearing this jumper and tying the VCCIO pin to 5V or any other IO voltage you need.
Board comes assembled with IC as shown.
Features:
- Implements full v2.0 USB protocol
- Needs no external crystal
- Internal EEPROM for device ID and Product Description strings
- Royalty-Free Driver support for Windows, Linux, and Mac OSX
Documents:
- FT232RL Breakout Schematic
- FT232RL IC Datasheet
- Eagle Files
- FTClean (for removing extraneous/old ports)
Drivers: FTDI Driver Page
Dimensions: 0.9x1.25"
Pricing
Comments
20 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.





























I can tell you, (and everyone else) this particular board is the best thing that FTDI created a chip for since they started the process of making USB to anything function chips.
I messed up my EEPROM with MProg, and I uploaded the default file. What can I do to make it work again like it did?
While I can see the differences, namely lower power consumption and (theoretically) easier programming, I can not see why the firm didn't simply create a new board number to accommodate this part number.
I have here both the board for the FT232R and now the one for the FT232RL and the differences are apparent.
Even the comments, including mine seem to be strangely wrapped around it. Although the threading seems to be broken.
The other USB boards don't breakout the RI pin.
I am new to this little board and I was wondering if you can connect this board directly to any usb com on my computer without any extra devices?
When you interface this board with your Atmega chip do you only connect RX,TX and ground?
Thank you,
Abraham
I basically want to route the information received by an rf module (http://www.sparkfun.com/commerce/product_info.php?products_id=8948) to a PC via USB. Is this the board/chip I need?
Thanks in advance
It also does not come with any documentation, except what's on the website.
I am using it to programm funnel I/O remixed, and it operates flawlessly.
I was even able to configure Arduino Alpha 0017 to recognize FIO remixed via this board... Too cool.
- two LEDs for Tx and Rx added,
- pin layout and pin description on back were changed,
Nice changes, I will add the new batch next my purchase.