Search
Product Info
Arduino ProtoShield Kit
sku: DEV-07914
Description: Riding on the waves of the very popular Arduino USB board is this small prototyping shield. Originally spawned with collaboration between the folks at SFE and ITP @ NYU, the Protoshield mates with the Arduino USB board and gives the user a small soldering area, two general LEDs, access to a BlueSMiRF socket, a general pushbutton switch, and most important of all - the Arduino reset switch is brought to the top level.This comes in kit form and must be soldered together by the end user. Please note - we do not ship assembly instructions! There are a few tutorials on assembly listed below. All soldering is through-hole (relatively easy) but always check your component orientation before soldering!
The kit is pictured with the bread-board option. We highly recommend this breadboard! See the related items below for all the colorful options of breadboards you have.
Kit Includes:
- 1x Protoshield bare PCB
- 2x Stackable Headers 6-pin
- 2x Stackable Headers 8-pin
- 2x 5mm Basic Yellow LEDs
- 2x 330 Ohm resistors
- 1x 10k resistor
- 2x Momentary push buttons
- 2x 0.1uF Ceramic Capacitors
- All Arduino pins are brought to the top level
- 5V, GND, and Raw pins are exposed as well
- BlueSMiRF socket for wireless communication between Arduinos
- 2 general use LEDs
- 1 general use button
- Reset button brought to top level
- Protoshield Schematic
- Arduino Home Page
- Assembly Tutorial by Bob Gallup
Pricing
Comments
13 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.









































http://www.flickr.com/photos/rsbohn/249994855/
Now to build something on it!
one weird thing though. The leads from the switch S2 contact the USB receptable on the arduino board. the tutorial points this out and recommends electrical tape to prevent a short. Seems like something that could be avoided in the design. if you take the shield off and on or it is anywhere it might be compressed you can be sure the sharp pins from S2 will go through electrical tape and short. I am looking for some kind of potting material or epoxy to ensure no short.
But seriously, being able to purchase the bare board by itself would be a very awesome thing.
As others have said the full kit is great for prototyping, but once you have a final design and you'd like to hardwire it you either have to desolder the headers or buy another full kit. The cost savings of one board would not be much, but if you're producing several copies it adds up quickly.
Also it would be cool if the Eagle files (brd and sch) were available for this board, to use as a starting point for creating custom shields.
Keep up the good work, SFE!
The analog inputs are numbered backwards from the arduino (NG & diecimila at least)!! You can go mad wondering why your sensors seem to be floating (they are - look under the shield at the real thing to get your terminal #'s right)
Also, the S2 button is not pulled down properly. It's on the PCB as Junction - resistor - switch - ground. Oops, unusable!
So the shield - good idea and all that, but whoever QA'd it needs to be let go!