Search
Product Info
Copernicus DIP Module
sku: GPS-08146
Description: The Copernicus is a great new GPS module from Trimble, but the SMD module prohibits immediate gratification. This DIP allows the customer to gain direct access to the pins on the SMD module. The Copernicus DIP breakout has an impedance-matched, end-launch, standard SMA connector that will mate with our SMA GPS antennas listed below.
Check out our GPS buying guide!
- Copernicus Manual
- Copernicus DIP Schematic
- Copernicus Eagle files
- SparkFun GPS Tutorial
- GPS Tutorial by Michael Simpson
Software:
Dimensions:
-
1.1 x 1.25" - 0.9" between pins (bread board friendly)
Pricing
Comments
7 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.



















This is the related link I found on the Trimble website:
http://www.trimble.com/embeddedsystems/copernicus.aspx?dtID=overview
Regards
Thanks for fixing the links !!!
The Trimble Studio is worth to try.
Regards
Jorge
-PCPete
I was wondering if there is an EAGLE library for this breakout board in the SparkFun library. I could not find it.
If there isn't one, could you please provide the distance between the two lines of pins?
Thanks!