Search
Product Info
Breakout Board for XBee Module
sku: BOB-08276
Description: This is a simple breakout board for the popular XBee product from Maxstream. This board breaks out all 20 pins of the XBee to a 0.1" standard spacing dual row header. The spacing between 0.1" headers is 0.5" making it breadboard DIP friendly. We highly recommend using the female sockets to avoid having to solder the XBee permanently to the breakout board. This is the PCB only. Please order the accompanying 2mm sockets (you'll need 2!) and 0.1" headers below.Documents: 5V Interface to 3V XBee module
Pricing
Comments
9 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.































I soldered in the 2mm sockets normally, and some of the solder ran through and into the holes that accept the xbee's pins. I could not get the solder out with wick, so the socket (and the board when i tried to desolder it) was ruined.
picture here:
http://picasaweb.google.com/marc.bayerkohler/Misc#5256440319164643730
you can see where some of the solder went through and filled the copper receptacles, so the xbee would not plug in.
Maybe Sparkfun could carry some of these with the Xbee sockets already soldered on?
I realise now that all that solder must have been going somewhere! At the time though I just kept pumping it in.