Search
Product Info
Color 24-Bit LCD 4.3" PSP 480x272
sku: LCD-08335
Description: These are original Sharp color TFT-LCDs designed to be used in the PlayStation Portable. 4.3" of beautiful 24-bit color with powerful LED backlight. 480x272 pixels - each pixel has RGB control. Data interface is 24-bit so start looking for a powerful controller (ARM7, ARM9, FPGA, etc).These are not OEM units or pulls! Check the photos. These units have original Sharp production barcodes, date codes, and LED backlight.
Documents:
Pricing
Comments
16 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.























I need the power adapter to connect the LCD to my plate prototypes.
Thank you.
español
»
inglés
Traducir
Important note to anyone thinking of using this LCD though:
You need 28 volts at 20 milliamp to power the backlight. Don't just connect it to your standard 5V supply... you're going to need a boost converter.
To sparkfun: You guys went to the trouble of making the LCD test board in the picture... why don't you sell it?
^ This link may work a little better
Please tell us what kind of ARM µC do have a compatible LCD interface.
Will you publish your breadboard harware and software ?
Can you do that, please ?
Thanks
Check out the video of the project I did with this didplay:
http://www.youtube.com/watch?v=zB6M_l4btpk
A LCD controller implemented on a FPGA device.
Cheers
http://dsp-cg-fpga.blogspot.com/2009/09/welcome-this-is-my-blog-about-fpgas.html
Very useful information, with connector part numbers given that some of the above people are looking for
Hope that helps
PLS bring its breakout board. WE ARE WAITING ON...
http://www.lcdinfo.com/products/usbd480-lq043.html
I haven't posted there, but if anyone could confirm the functionality of this...