Search
Product Info
Bluetooth® SMD Module - SparkFun
sku: WRL-08474
Replacement: None. We don't have a direct replacment for this product. It has been discontinued. Check out our other Bluetooth SMD modules. This page is for reference only.
Description: The SparkFun Bluetooth® module is a module designed to replace serial cables. The Bluetooth® stack is completely encapsulated. The end user just sees serial characters being transmitted back and forth. Press the 'A' character from a terminal program on your computer and an 'A' will be pushed out the TX pin of the Bluetooth® module.
This new module from SparkFun uses the BGB203 IC from NXP. The BGB203 is a powerful IC with a flexible AT command set.
Please note: The SparkFun BGB203 based module will be replacing the phased-out Mitsumi module. The new BGB203 has a lower cost and a more robust AT command set. The shape, size, and pinout of this module is the same as the Mitsumi part. The only difference between the two modules is the SparkFun module has an active low output for the Status pin.
Features:
- Fully configurable UART
- UART Data rates up to 1Mbps
- Low power sleep mode
- Compatible with all Bluetooth products that support SPP (almost all do)
- 3.3V operation
- Status pin
- Bluetooth v1.2 compatible
- Class 1 power output
Documents:
Pricing
Comments
11 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.




















Is it possible via bluetooth connection in "Hyper Terminal" ?
Thanks
Note that the connectors down the edge seem to be more like 47mil pitch, rather than the 45mil stated in the the dimensional document above.
Now just need to work out how to change baud rate...
There is more documentation under this part WRL-08461. It's basically the SMD mounted on a breakout board. The breakout board has all of the pins listed.
Good luck
First off here is a very useful link: This is the user guide for the Philips BGB203
http://www.robotshop.ca/PDF/BGB203_SPP_UserGuide.pdf
---
SL: There is more documentation under this part WRL-08461. It's basically the SMD mounted on a breakout board. The breakout board has all of the pins listed.
---
Great addition. Thank you for mentioning that
---
ROBOSTEAL: Caution: the dimensional drawing linked on this page as of 2009.5.9 does NOT reflect the parts shipped by SparkFun.
---
The part has not changed nor been modified. I apologize that you may be experiencing issues with your foot print. However I would recommend contacting Sparkfun Technical Support prior to posting up a disclaimer.
Neither the part or documentation have been modified. Hope this helps you guys out.
Thanks!
Can someone tell if I can use this module without a microcontroller. I want to use it as an adapter with the ID-12 rfid reader(TTL output ) , so that i send the data from the reader directly to a PDA.
Thanks in advance