Search
Product Info
Conductive Thread - 117/17 2ply
sku: DEV-08544
Description: Conductive thread is a creative way to connect various electronics onto clothing. This thread can carry current for power and signals. While not as conductive as traces on a printed circuit board (PCB), this thread makes wearable clothing 'wearable'!This is a finer thread that can be used in standard sewing machines. Resistance is about 82 Ohms per foot. Spool contains 1 oz of thread, about 150 yards.
Pricing
Comments
3 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.
























I then tested the thread with a multimeter straight from the spool and it worked as specced for short lengths of < 30cm, but has random breaks with resistances in the million ohm region. This made the thread completely useless to me.
I'm trying to wire up a bunch of sensors on the back of a glove, and I'm having to insulate the stitches with bugle beads and wrap all the knots in embroidery floss. It's a lumpy, heavy mess.
Whenever I trim the stuff, I get an explosion of shreds that I then have to pick off the fabric with tweezers or a piece of tape.
It's wretched stuff.
For what I need, the product works fine but what will SFE do about the quantity issue?