Search
Product Info
Graphic LCD 84x48 - Nokia 3310
sku: LCD-08629
Description: This is a small monochrome LCD 84x48 pixel display that was used in the immensely popular Nokia 3310 phone. This is a very low power display (less than 1mA) but has no backlight. Great for low power remote node applications.Search google for Nokia 3310 LCD and you will find lots of documents and resources including pin outs.
This product includes a small electret speaker that can be driven from GPIO pins on a microcontroller.
Documents:
Pricing
Comments
12 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.












http://fuzzymonkey.net/software/avrmicrocontroller/nokia-3310-breakout-v1.0.zip
Note, the hardwork was done by pay.c at the AvrFreaks.net forum. He shared his Eagle part in this post. That post has a PDF of a single sided board for etching which is probably the way to go for anyone into that.
Also, I have not ordered the board yet so consider it untested.
http://tinkerish.com/blog/?p=39
Don't worry about the breakout, just solder wires directly, and then hot glue the connections.
The contrast doesn't look bad, I would just like to be able to change it if needed.
If you use a 5x5 font with 1 pixel of spacing between each character, this equals to a 14x8 display for only 4.95$USD. A character-based LCD display would cost at least 10-15$ for 16x2 characters, and would be much bigger.
If you prefer to use a 5x7 font, again with 1 pixel spacing between characters, you get a 14x6 display, which is still three times as many rows as a 16x2.
And you also have the bonus of being able to do graphics along with your text.
Sparkfun should make a small board for these displays, unless it ends up doubling the cost of each LCD.
SparkFun: how about a custom PCB where we can take the LCD out of that plastic cellphone assembly and have a regular, breadboard-friendly 0.100" header?
Jaapio