Search
Product Info
CMOS Camera - 1300x1040
sku: SEN-08668
Description: The TCM8240MD is a high quality, very small 1.3 mega-pixel color camera from Toshiba with the standard data+I2C interface. The nice thing is that we have a complete datasheet on this camera along with a good supplier. This camera is also unique in that it offers on-board JPEG compression.
Features:
- Small size
- 2.8V Supply
- Up to 15fps
- 1300x1040 pixel resolution
- Built-in color filter
- 1/3.3 inch optical format
- Auto luminance control (ALC)
- Auto white balance (AWB)
Documents:
Pricing
Comments
10 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.
















http://picasaweb.google.com/nachox2002/Fotos_placas#5222075215944573762
Is a breakout board (not a beta release ) available, if so, where can I get it ?
Check the forum:
http://forum.sparkfun.com/viewtopic.php?t=10314
The bottom line is that it is poorly documented and no one (that we know of) has been able to get valid images off of it .
Still no one has been able to get JPEG images off the camera. Also note: JPEG compression is only available for the full 1.3MP images, not for the smaller image sizes.
Keep in mind that this camera is poorly documented - and the datasheet is written in "Engrish."
I am a newer one to start the project with TCM8240. Plz anybody tell me the hardware configuration of this device. also the commands to I2C bus in order to read the output from the data lines
thanx
As has been stated, the issue here is poor documentation.
We have contradicting datasheet vs appnote vs state cam is in when booted.
We also have multiple registers documented or otherwise that have to be adjusted to suit the resolution you select.
That said, it is possible to get data from it and I have successfully grabbed both 1280x960 and the maximum 1280x1024 from the camera. The quality of the images are as of yet appaling due to the forementioned registers.
I am sure that with the right settings this cam would be suitable for high powered mcu's like the AVR32. (I am using AVR32 on NGW100.)