Search
Product Info
FM Receiver Module
sku: WRL-08770
Description: This is a very small single chip FM receiver module found in many portable media players. Based on the AR1010 IC from Airoha, the FM receiver uses a simple command set over an I2C or SPI interface. Crystal and supporting components are all on board, all you need to attach is an antenna!Features:
- 3.3V @ 11mA
- 76-108MHz supported
- 100mV audio output
- Stereo output
- FM Module Datasheet
- Example AR1000 ATMega168 Code for reference
- AR1010 Datasheet, Programming Guide, and sample C code available upon request
- TEA5767 Datasheet for reference
- Application Note for reference
Pricing
Comments
13 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.






















http://www.rockbox.org/twiki/pub/Main/DataSheets/application_note_tea5767-8.pdf
http://www.rockbox.org/twiki/pub/Main/DataSheets/application_note_tea5767-8.pdf
Use it to test the functionality of the AR1000! have a look at the ReadMe file for more information on how to use it.
Also please note that right now the jumper on the board does not come soldered, this will change! and it will come jumpered very soon. updated pics will follow.
To use the example code, the jumper must be closed, so if you get one that is not soldered please solder it yourself or close the connection some other way.
I suppose that the antenna could be created on a PCB: are there any ideas about the geometry & dimensions??
Thanks a lot,
Settuz