Search
Product Info
Breakout Board for VS1033D MP3
sku: BOB-08792
Description: The VS1033D-L is a great MP3 decoder, and with this breakout board, it's easy to drop it into any project. The VS1033 is capable of decoding MP3/AAC/WMA/MIDI audio and encoding IMA ADPCM. Can drive 30 Ohm headphones with no additional power supply.
Features:
- Separate Audio and Digital 3.3V supplies
- Onboard 12.288MHz oscillator
Documents:
Replaces: BOB-00519
Pricing
Comments
16 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.
























Does this board contains the decoder chip or do i
have to order it separately?
Thanks.
the pictures are wrong, this comes on a red PCB identical to the VS1053 breakout board
Also, what's the digital supply voltage? Will I need level translators for the SPI bus lines? (VLSI's website is currently down, so no data sheet right now)
Thanks for your help.
I assume the output of those are 3.3V based again upon
the schematic. I can only assume I can deliver 5V which
would be regulated to the 3.3V however I have no idea of
the regulators as they are not defined in the schematic.
SO....could anybody provide a bit more information so I don't let the smoke out of something????
We have been able to get the board to work when we create a solderblob that connects TEST pin 32 to CVDD3 pin 31. Make sure you've got a fine tipped soldering iron for the job!
I worked with the VS1033D board and it had extremely intermittent operation. If you moved a finger near it, it would emit static. But now I know it's because the test pin was floating.
Another warning: CVDD is powered at 3.3V (same as IOVDD) but the VS1033D datasheet says 2.7V is the maximum. Not sure what the implications might be, but it's definitely out of spec.