Search
Product Info
XBee Explorer Regulated
sku: WRL-09132
Description: The XBee Explorer Regulated takes care of the 3.3V regulation, signal conditioning, and basic activity indicators (Power, RSSI and DIN/DOUT activity LEDs). It translates the 5V signals to 3.3V so that you can connect a 5V (down to 3.3V) system to any XBee module. The board was conveniently designed to mate directly with Arduino Pro boards and with the FTDI Basic boards for wireless bootloading and USB based configuration.This unit works with all XBee modules including the Series 1 and Series 2.5, standard and Pro versions. Plug an XBee into this breakout and you will have direct access to the serial and programming pins on the XBee unit and will be able to power the XBee with 5V.
This board comes fully populated with 3.3V regulator (16V max input), XBee socket, four status LEDs, and a diode to allow 5V systems to communicate safely with the 3.3V XBees. This board does not include and XBee module. XBee modules sold below.
Add a couple XBees, and a USB Explorer and you've got a great gift for that special electronics geek! For more gift ideas check out our SparkFun Gift Guide!
Documents:
Wow there are a lot of XBee modules! Here's a breakdown:
Series 1: Good point-to-point (300 ft)
Series 1 High Power: Point-to-point and decent range (~1 mile)
Series 2.5: Multi-point networks (300 ft)
Series 2.5 High Power: Multi-point and decent range (~1 mile)
900MHz: Longer range (~6 mile)
900MHz High Power: Super long range (~15 mile)
Pricing
Comments
19 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.






























@Valen - I question this too, as there's no level shifter shown in the schematic. Digi says (but not in the manual from what I've seen :-() that the I/O pins are *NOT* 5V tolerant, so I don't understand how/why they can say that above, at all.
You both might take a look at Ladyada's XBee adaptor kit,
http://www.adafruit.com/index.php?main_page=product_info&cPath=29&products_id=126
She's got a level-shifter on her UART and reset pins, and her V-reg is a little beefier at 250mA. You need to decide for yourself if/how 250mA will work for whatever you're using it for.
As for level-shifting the GPIOs, you're on your own.
Thanks in advance
it would be nice if the explorer also provided cross-wire protection. if someone accidentially crossed the lines (conecting tx-tx instead of rx-tx) the tx pin might get burned.
and a question:
can the tx-pin get burned if its accidentially connected to the tx of a 3.3volt device or is it only a risk with 5v devices?
What model of voltage regulator is used?
thank you!
You can view the voltage regulator's datasheet here.
The maximum supply voltage shouldn't exceed 16V (maximum rating on both the 10uF capacitor and max operating voltage of the regulator). Be really careful if you're going to run it that high though, things could get toasty!
-techsupport at sparkfun dot com
Also - it appears the XSC pin assignments vary from the XBee and XBee Pro modules, so I'm not sure if any common Xbee regulator board will work with the XSC.
See topic
http://forum.sparkfun.com/viewtopic.php?p=84374
I can't explain exactly why, but when using this board as shipped, I would received only null (0x00) for every byte transmitted and I couldn't access the module at all with XCTU (the digi configuration software). I know the setup was good because both worked just fine with 2.4GHz (series 2.5) modules. After someone else suggested shorting out the diode, I soldered it up and now everything appears to be working fine.
Thanks for the original comment AdamB, would never have thought of this if you hadn't posted.
Jon
Jon