Search
Product Info
Triple Axis Accelerometer Breakout - ADXL335
sku: SEN-09269
Description: Breakout board for the 3 axis ADXL335 from Analog Devices. This is the latest in a long, proven line of analog sensors - the holy grail of accelerometers. The ADXL335 is a triple axis accelerometer with extremely low noise and power consumption - only 320uA! The sensor has a full sensing range of +/-3g.
There is no on-board regulation, provided power should be between 1.8 and 3.6VDC.
Board comes fully assembled and tested with external components installed. The included 0.1uF capacitors set the bandwidth of each axis to 50Hz.
Not sure which accelerometer is right for you? Our Accelerometer and Gyro Buying Guide might help!
Dimensions: 0.7x0.7"
Documents:
- ADXL335 Data Sheet
- Schematic
- Example 3D cube project using a PIC
- Wiring Example
Pricing
Comments
11 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.


























I tried with the self-test pin but it's completely gone... the other 2 axis work fine... has anyone else had this problem??
In the text they say use the voltage between 1,8 and 3,6 VDC.
In the Schematic stand 5 V DC
What to use?
I'm thinking about ordering one, I have 2 ideas on how to fixate it, but they are both meh.