Search
Product Info
Geiger Counter
sku: SEN-09298
Description: This is a USB powered Geiger Counter equipped with an ATMega168 that can be programmed in circuit using one of the programmers below. Simply plug the unit into USB (make sure you have FTDI drivers installed), open a terminal program to the correct COM power at 9600bps, and you will see random bits being generated from the random background radiation. Here at SparkFun, on average, we get about 20 counts a minute.Check out the random number generating Geiger counter tutorial for more information.
ATTENTION: While the Geiger counter is powered and the switch is in the ON position, the board contains exposed high voltage components. In order to turn the unit off, you must flip the tube power switch to OFF while the USB cable is plugged in or while the board is still connected to your power supply. The reason being; when you move the switch into the OFF position, the high voltage lines are bled out through a resistor connected to ground, more information on this is in the tutorial.
A project box or enclosure is suggested. Do not touch the end window of the Geiger tube and do not to touch any conductive region inside the area marked HIGH VOLTAGE when the Geiger tube is powered ON. An enclosure is not absolutely necessary, but if you choose not use an enclosure, remember to be extra careful with the end window and high voltage regions.
The Geiger tube comes with a red boot to protect the end window during, production, handling, and shipping. The boot should be removed if you are needing to detect alpha particles. However, you should still see activity from gamma and beta particles even with the boot on.
For older revisions with a bleed button: Remember to always hit the bleed button with your power supply connected, after the tube power switch is moved from the ON position to the OFF position.
Features:
- 5V@30mA input
- LND712 Geiger tube
- ATMega168
- FTDI USB
- Power and status LEDs
- TTL output pin from tube
Documents:
Pricing
Comments
17 comments
Feeds
Currency
Display prices in
Feedback
If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.





















You'll want to get a radiation source to increase the number of readings. I recommend United Nuclear:
https://unitednuclear.com/index.php?main_page=index&cPath=2_5
This Geiger tube is well suited to have an isotope disk source placed directly in front of it's detection window. But, beware of maximum detection rates.
Also, Nuclear Safety for kids:
http://meaning.com/wiki/Image:Ghosted-eliz-cs-137.JPG
I do not have the expertise necessary to know whether they're right or not but if they aren't (or are) you might want to comment on the article yourself! There is plenty of praise in the comments, too.
Opto-isolating the high voltage from digital line is a great idea and we will take that design suggestion into consideration for the next rev.
However, the current design works great and I have been using my 1st proto since earlier this year without problems. Isolating the high voltage from the digital might not be completely necessary when you take extra precaution with physically isolating the digital line from high voltage lines.
Your suggestions are greatly appreciated, keep 'em comin!
Is there some sort of liquid paint-like substance that I can purchase, which this thing will detect?
TIA.
These systems are expensive but do the job very well.