Skill level:     Beginner
 

Reflow Skillet

by Nate  |  
July 1, 2006  |  

I've been reflowing SMD parts on PCBs for around a year now. Spark Fun has barely had the capitol to invest in a hot-air rework station, let alone pick and place machines and industrial reflow ovens. Luckily, as business has increased, revenue has allowed us to purchase a few bottom-dollar machines to help with manufacturing. I'm here to tell you, it was all a waste of money...

Don't get me wrong, there is the correct way to manufacture 10,000 units of a caller-ID controller board, and then there is the Spark Fun way. If you're reading this, you're like us - strapped for cash and in need of a good way to reflow PCBs.

Here is a tutorial that will break down the different approaches to SMD reflow soldering, what we've learned, and what to steer clear of.

As always, this stuff can kill you, burn your house down, or make your basement smell pretty foul. Don't try any of this at home - wait, you are at home. Well, just take everything we say with a grain of salt.

SMD Reflow Tutorials:

There are five ways to solder SMD parts that I can think of:


Hand Soldering - 

Hand soldering is cheap (no extra equipment needed). You will need a decent iron, but nothing else. $100 is pretty standard for an iron although $50-$2000 is possible.

New users to soldering SMD devices are always intimidated by soldering itty-bitty leads. Believe you me, it can all be hand soldered.

Common questions:

  • Do I need a microscope?

Maybe. I've never used one but Pete does. With a little practice, we can see disconnects and color variations that indicate problems with the naked eye.

  • Do I need a super fine tip?

Probably not. Don't even think about trying it with your $10 Radio Shack fire starter! But a conical tip of small size works fine. A heftier tip can be beneficial in some cases (helps to move solder blobs).

  • I certainly can't hand solder XY type package!

No really, you can! No matter how small the pitch, even leadless QFN packages, can all be soldered with some solder wick and some solder ball chasing. It's not easy and not fast, but it can be done. The only exception is BGA which I've never tried with an iron. But get creative! All you have to do is heat up the overall area. Soldering from the back side of the PCB using vias as heat ducts has worked for other people.

Over all, hand soldering is the way to do it when other means are not available.

Pros:

  • Soldering equipment most likely to be available

Cons:

  • Very slow
  • Boards get dirty with all the flux running around
  • Heat stressing can lift pads if the soldering student is new to soldering

Toasting -

Using a toaster oven has been shown to work in many cases. A $50-$100 toaster oven from your local Wally World can do quite nicely. The Seattle Robotics Society's report on Toaster Oven Reflowing covers the process nicely. I've even built up a controller board to try to mimic the real reflow oven profiles.

Ben and I have found that many plastic connectors have low melting points while other connectors (SMD USB connectors with metal housings) have very high reflow points. This was a major problem on the GM862 EVK v2 boards. Time and time again, either the USB connector would fail to reflow because of the metal housing reflecting the heat, or we would bake the board so long that the USB would reflow but the plastic Camera connector would be completely hosed. In other words, you have to destroy the plastic connectors or have larger connectors pop off in your hand. The main culprit in our case was the over-head heating elements in our industrial reflow oven. Since our toaster oven has elements on both top and bottom (the top elements heats up much faster), a toaster oven would have the same Achilles heal, melting the softer components on the top side of the PCB.

Here we have the initial test of the Spark Fun Oster Toaster. Starting from 25C, the ramp is 225C in 5min or 45C/min = 0.75C/s. This is actually pretty good. The commercial reflow ovens are 1-1.5C/s. The massive drop at 5min is when the front door was opened. The toaster can actually hit 250C without any problems.

In the end, toaster ovens work, but they are too dependant on external control or attempting to view inside the little window waiting for something to happen. Over-head elements run the risk of melting plastic connectors to the point of destruction.

Pros:

  • Pretty cheap
  • Works well

Cons:

  • Difficult to know/see when to open the door when the boards have fully reflowed
  • Can melt plastic connectors

Industrial Ovens -

Don't get me started. We dropped $2300 on a reflow oven from Madell Tech because we didn't know any better. It was a good lesson learned. The oven is fairly large so shipping was pretty steep. The unit runs on 220V and came with some incompatible Chinese plug on the end.

Some pictures:

The profile can be set to any temperature over any length of time through this fancy LCD and a couple tactile buttons.

As you can see, the tray is pretty large. The oven has fans built in for cooling. The elements are IR which heat very quickly allowing the temperature to be monitored very closely. The slim brown thing is the temperature sensor that is supposed to be taped to every PCB that is reflowed - something we've never done.

As stated above, this thing is a problem because there are cold spots where the USB connectors never reflow. If we tweak the profile up high enough to reflow the USB connectors, the plastic connectors melt. We've had repeatability problems, etc, etc. We continue to use the oven for large batches. It could easily be an operator error - we may be missing something simple. Either way, we are happier with our $30 hot plate.

Pros:

  • Interface is beautiful
  • Larger capacity
  • Absolute profile control

Cons:

  • Runs on 220V
  • Expensive
  • Very large footprint

Hot-air Rework -

This is a favorite around the office. Using these cheap rework stations saves time and money.

Common questions:

  • Which nozzle do I need?

Actually, we stuck the basic small circular nozzle on there and have never taken it off. The hot air just sort of flows everywhere heating of the immediate area of the PCB.

  • Which type of unit do I need?

I noticed the other day, the digital stations will tell you precisely what temperature is leaving the nozzle, but what is the temperature of the PCB? Who cares? Most applications dictate that the temperature be lower than some threshold, but the overall temp does not matter. All that matters is that it is hot enough to melt all solder joints at the same time. Given enough time, you can truly warp a PCB, boil off the solder mask, etc. It's a tool that takes practice and learning. Nothing too major - we love em!

Pros:

  • Decent price for great versatility

  • Can save almost any IC/part

  • Can fix almost any messed up solder job/placement problem

Cons:

  • Could burn your house down - no auto shut-off

  • Using a hot-air gun for reflowing can take a long time (5 minutes a board)


Hot Plate Reflowing -

Finally we get to the point of this tutorial... After playing with all of the above, we were still being forced to hot-air fix some boards, solder on others, and had even more problems with others.

The reflow oven was melting some boards and not reflowing others. Hot-air was taking far too long, hand soldering was out of the question. The toaster oven was cheap, but would have similar problems to the IR oven. Finally, Ben and I wondered why we couldn't use a hot plate to heat just the PCB - this would protect the plastic parts and should reflow the USB connectors better (heat transfer is better because the IR heat was bouncing off the metal housings whereas the hot plate heats the PCB directly). $32.44 and another short trip to Target and we've got ourselves a hot plate!

Holy smokes - I could take this thing back in 3 months!

Okay, so it's actually a hot skillet. There was a hot-plate for $19.99 but I decided it was a bit small and opted for the larger skillet with lid (might help, right?).

So I have Ben whip up a Lassen iQ breakout board with the evil USB connector and tricky USB CP2102 IC. We grab a temp gun to watch the temperature of the skillet. The dial controller reads up to 450F(230C). This should be more than enough...

So we plug 'er in and let 'er go. It was probably 2-3 minutes of staring before the temperature hit ~200C and we noticed the smaller components reflow. As expected, the USB connector took an additional 20-30 seconds of ramping up heat. Finally, after the USB solder connections looked good, shiny, and liquid, we turned the dial to off and waited for the board to cool. A quick test and the board passed on the first try! The USB connector was soldered solidly to the board and all plastic parts survived. The only noticeable problem was the silkscreen on the plate side (PCB bottom) was slightly lightened as if some of the ink had been removed - though it was still white...

How about some pictures? This is the CP2102 breakout board, in a panel of 4x3.

V-scored PCB before paste application. We use Kester Easy 256 solder paste. For more information about how to stencil solder paste - have a look at our solder paste tutorial!

The hot skillet reflow-er

Baking - at about 100C. Notice how all the paste looks grey and dusty.

The Power LED and one side of the tantalum cap have reflowed ~200C

All small components are flowed - ~210C

USB now reflowed ~225C

The pictures don't show it, but it is actually very easy to tell when the solder paste has turned liquid.

This panel was much trickier to reflow as the skillet has a circular heating element. The center is the coolest part. By sliding the PCB around (wonderful Teflon) I was able to position the various problems spots to a hot spot in the skillet. The smaller, circular, $20 unit from target may have a better element.

I don't think anything can replace the large scale, multi-zone, IR/convection reflow ovens. But I could by 100 hot plates at $30 a piece before coming close to the price and performance of a traditional reflow oven.

Pros:

  • Low cost

  • Works well

  • Available anywhere

  • Small footprint

  • Operates on 110V

Cons:

  • Non-uniform heating area

  • Skillet sides can burn arms


Email us! spark at sparkfun.com

Back to Tutorials

 

Comments

14 comments


Log in to post comments.

by
josheeg's rank:
+4.5
|   September 30, 2008 at 11:58 AM
Comment rating:
0
Any oil that does not burn at low temp my dad used vegi I would use peanut. But he used it to make the heat transfer better to the metal so the board burned less when he removed parts.
But you must only use a little.
by
josheeg's rank:
+4.5
|   October 11, 2008 at 2:35 PM
Comment rating:
0
Why not his from mouser for small quantity silver solder paste?
557-7459



7459


Wahl Soldering Irons/Accessories SILVER SOLDER PASTE Page 2,081 In Stock

Click
to
View
1: $5.03
12: $4.29
andrewwynn's rank:
+1
|   November 22, 2008 at 11:51 PM
Comment rating:
0
LIFE SAVER!

I bought the exact $20 target hot plate, and after a couple tests with layering different heat-spreader plates and testing different power levels (burned up one board pretty bad)... figured out a perfect solution.

I use a 1/8" piece of aluminum between the hotplate and circuit board to even out hot-spots..

I monitor the temperature either with IR thermometer or thermocouple with my fluke multimeter.

I use the profile shown here:
http://images.pennnet.com/articles/smt/cap/cap_131774.gif

I start a stop watch and basically dial the power to achieve 150C in about 90 seconds, about 180C in 3 minutes.... then turning up power to full power for about 30 seconds and then off... it gives me a spike of about 220C, and has been working perfectly.

I made a test stencil myself.. see the stencil thread.

-awr
teqdruid's rank:
+2.2
|   January 12, 2009 at 8:36 PM
Comment rating:
0
Great ideas guys! I recently bought a hot plate and an soldering boards in a 3/4" aluminum plate I place on top. I have to do the component placement on the plate and on the hot plate, and it takes forever to cool down. Does anyone know of an adhesive I might use to secure the components elsewhere then move the board?

By the way: be careful with Teflon! Teflon has been "shown" to give off toxic and carcinogenic particulates starting around 464 degrees Fahrenheit (240 C) which is why I'm using aluminum. I've heard this as rumor and hear-say, and the quick Google sources don't look terribly reputable. I dunno if these claims are true or are FUD, but I've found the aluminum plate works well.

~John
by
doctek's rank:
+3.3
|   January 31, 2009 at 4:09 PM
Comment rating:
0
This approach works great. Because I wanted a bit more heat (I use lead-free solder), I used a hot plate. But I found that I needed much better control of the temperature than the hot plate had. For a detailed explanation, including how to build the controller, check out this Instructable.
http://www.instructables.com/id/Extreme_Surface_Mount_Soldering/
by
Joe P's rank:
+1.5
|   February  8, 2009 at 10:47 AM
Comment rating:
0
Okay, now I'm nervous... I've never worked with surface mount stuff, read this article, and finally stopped being a chicken and layed out and ordered a PCB, solder paste, and the parts to populate it. Now, in the down time while I wait for my BatchPCB order, I discover that there's a specific heating profile to reflow solder...

How critical is the profile? In my PCB order, I only ordered one copy of the surface mount board I layed out. I was thinking I could put the board on the skillet, turn it on, and when everything's shiny, turn it off... I'm going to ruin my board, aren't I?
by
Cory's rank:
+1.9
|   February 20, 2009 at 8:25 PM
Comment rating:
0
Using a hot plate is easier than you think. Ideally you want to try to keep the hot plate at about 230 dec C (for lead solder), so let it warm up first before putting your board on. When you place your board on, I find it helps to hold it down so it makes good contact with the hot plate. I use two pairs of tweezers for this. Then, once all the solder has reflowed, lift the board off the hot plate and let it cool. Easy as that. Don't worry about the temp profiles. Don't leave it on the hot plate while the hot plate cools down.
by
AJP's rank:
+1
|   February 13, 2009 at 4:31 PM
Comment rating:
0
One more thing, safety. Don't forget to go to wal-mart and buy a cheap hot-plate hood. A 8" wire-mesh cooking strainer with a handle will work fine.
by
Davardo's rank:
+4.2
|   June 17, 2009 at 10:14 AM
Comment rating:
0
Can we include the occasional DIP (thru-hole) component or do that as a separate operation?
Mast3rbug's rank:
+2.7
|   July 17, 2009 at 10:11 PM
Comment rating:
0
I use an heatgun with a grill. Take about 3 minutes for 8x11 pannel.

It's the best for me.
by
jstone's rank:
+1.2
|   July 21, 2009 at 9:40 PM
Comment rating:
0
Will though hole also work with this method?

(I saw someone ask this, but there was no reply)
JohanAdler's rank:
+0.85
|   August 11, 2009 at 11:30 PM
Comment rating:
–0.15
One very old trick for getting an even heat distribution is to put a layer of clean dry sand at the bottom. I think about 1 cm (0.5") would be fine. The sand will spread the heat and you will get a "softer" and more evenly spread heat.

Since the sand will also retain or store heat you will not be able to accomplish any high speed changes in temperature, but I do not think that will be a problem. The sand is dry so there should not be anything to clean from the soldered boards unless some paste has found its way to the bottom side.
robotjosh's rank:
+1
|   December  7, 2009 at 10:56 PM
Comment rating:
0
Fantastic method! Much better than hot air for populated boards, in my opinion. After a few good runs with a $20 hot plate, I found an old scientific hot plate like you'd find in a chemistry lab, and they seem to have very good temperature uniformity and stability. The downside is cost if you buy them new, but if you can find one used or surplus they work very well for this!
Chimerahitman's rank:
+1.2
|   January 29, 2010 at 1:08 PM
Comment rating:
0
Hmm... I don't know if it is to late, but I was trying to do solder paste soldering with a toaster. It has heating elements on top and bottom if you lay it on its side.

I did some "temperature tests" and saw that it goes up to 250 in just about 1-2 mins. I guess toasters could be thee next big thing :)

All that is needed is control the heating up time, or reflow profiles. I didn't use any actual solder paste, and I tried it with just a copper clad with no circuit and cut a piece of my soldering wire. The only problem, i think, is that the clad seems to smoke before the solder, that is without any temp controling, just setting it on and wait till it hits 250.

Also, it does go up to 320 but it takes a while to get there after going up to 280.

Feedback

What's on your mind?

Please include your email address if you'd like us to respond to a specific question.

submit


If you would like to tell us more, you can fill out our form if you need some psycho-suggestive questions. Go to the form.