Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
With improved thermal features to support the higher peak power consumption of Raspberry Pi 5, it integrates a variable-speed…
The Raspberry Pi 4 Desktop Kit (8GB) includes everything you need to turn any monitor with an HDMI port into a desktop PC.
This 2x20 "tall" header has the same number and spacing of pins as a Raspberry Pi and provides your board with the ability to…
The Mountable MI:pro is a simple and compact protective case for the micro:bit.
The Argon ONE M.2 case features an M.2 interface for using M.2 (Key-B or Key-B&M) SATA solid state drives (not included).
Sometimes all you need is a simple but durable carrying case for your parts or projects.
These are our small, beefy aluminum enclosures, which have been built tough enough to withstand a truck. This 2mm-thick, die-…
The Raspberry Pi Zero Case has been designed to fit both the Pi Zero and the Pi Zero W. These official cases consist of sever…
The official case for the Raspberry Pi 4 from Raspberry Pi!
The SparkFun Raspberry Pi 4 Desktop Kit (4GB) includes everything you need to turn any monitor with an HDMI port into a deskt…
This sturdy carrying case is great for carrying anything from tiny components to medium-sized tools.
If you're looking for a fully-featured Raspberry Pi 4 case, then look no further than the Argon ONE Pi 4 Raspberry Pi Case.
These are our large, beefy aluminum enclosures, which have been built tough enough to withstand a truck. This 2mm-thick, die-…
The MI:pro Protector is a simple and compact protective case for the micro:bit.
This is the official case for the Raspberry Pi 3 Model A+ (it also fits the Raspberry Pi 1 Model A+ as well).
The Raspberry Pi is everybody's favorite little computer, the last thing that you'd want is for something bad to happen to it…
Tynker and BBC Learning take coding to the next level with a programmable HiFive mini-computer and guided lessons covering Bl…
The Argon POLY+ Raspberry Pi 4 Case uses a three piece snap-fit plastic design to protect your Pi 4 in a cost-effective way.
This is a basic baseplate for the Raspberry Pi 3 B+. The baseplate is designed for the RPi to remain on the attached via fric…
This metal enclosure finished in SparkFun Red will help protect your electronics from harmful contact from outside sources.
Ergonomically designed for hand-held comfort.