Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
RFM95CW is an ultra-low-power, high-performance LoRa transceiver for various frequency of 137-1020 MHz wireless applications.
The EM-506N5 GNSS module features high sensitivity, low power and ultra small form factor.
The MicroView is the first chip-sized Arduino compatible module that lets you see what your Arduino is thinking using a built…
The Artemis Module from SparkFun is the first FCC certified, open-source, Cortex-M4F with BLE 5.0 running up to 96MHz and wit…
Based on the 16MP Sony IMX519 sensor, this new camera module gives all Raspberry Pi hackers every bit of power they need to b…
The DYScan DE2120 is one of the coolest little barcode scanners we've ever seen. This tiny "scan engine" will read 20 differe…
Raytac’s MDBT50Q is a BT 5.2 stack (Bluetooth low energy or BLE) module designed based on Nordic nRF52840 SoC solution.
ESP32-C6 is Espressif’s first Wi-Fi 6 SoC integrating 2.4 GHz Wi-Fi 6, Bluetooth 5 (LE) and the 802.15.4 protocol.
The radiometric Lepton has 80x60 active pixels to capture accurate, calibrated, and non-contact temperature data in every pi…
The Leopard Imaging Camera is a 136° FOV camera module designed for use with the NVIDIA Jetson Nano Developer Kit.
RFM97CW Sub-GHz radio transceivers are ideal for long range wireless applications.
This module allows a designer to leverage the Raspberry Pi hardware and software stack in their own custom systems and form f…
The Espressif ESP32-C3 is the next version of the popular ESP32 Bluetooth and WiFi enabled module.
The ESP32 WROOM MCU Module with PCB Antenna is a powerful, generic WiFi+BT+BLE MCU module that targets a wide variety of appl…
It's best to think of the ESP32-S2 WROOM Module as the next step in the ESP32 WROOM module line.
The RN-52 module from Roving Network is an audio module that provides a highly integrated solution for delivering high qualit…
The ESP32-WROOM-DA module achieves high-quality, wireless connectivity across large areas, using two complementary PCB antenn…
The ESP32 WROOM MCU Module with U.FL is a powerful, generic WiFi+BT+BLE MCU module that targets a wide variety of application…
The BMD-34 series are advanced, highly flexible, ultralow-power multiprotocol modules that enable concurrent Bluetooth 5, Thr…
M6E-Nano’s wide RF output range (0 dBm to +27 dBm) is important for the read/write requirements for RFID-enabled printers a…