SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:26:01-06:00SparkFun ElectronicsCustomer #56502 on Scratch Programming with the PicoBoardCustomer #56502urn:uuid:3565b3ae-2199-9c1b-28d9-c25fa8471b4d2013-05-06T08:12:17-06:00<p>You might be able to connect scratch through python to the hdl code using this library <a href="http://bit.ly/RWr96u" rel="nofollow">scratchpy</a></p>
Customer #158196 on Scratch Programming with the PicoBoardCustomer #158196urn:uuid:e62084f7-8d7c-74cd-62c0-83d972f44aac2013-05-01T18:42:32-06:00<p>This is awesome. :-D<p>You should also really check out Tynker - pretty much Scratch in a browser.</p><p>http://tynker.com/</p><p>it's a scratch variant that is in a bunch of schools already being used by children. I'm going to investigate if it can be hacked to talk to this board through some kind of bridge</p></p>
Colecago on Scratch Programming with the PicoBoardColecagourn:uuid:f4350e53-34c4-fa16-6576-849a67ad67512013-05-01T15:42:05-06:00<p>Is scratch the direct result (extension) of Google App Inventor? I think it was handed off to MIT, and this looks pretty similar.</p>
LC on Scratch Programming with the PicoBoardLCurn:uuid:4459f26c-52e1-b5b5-bd49-8cfc95d9c2872013-04-30T14:48:24-06:00<p>I haven't played around with it too much but you may be able to connect Simon to <a href="http://seaside.citilab.eu/scratch/arduino" rel="nofollow">"Scratch 4 Arduino".</a><p>You can also look at <a href="http://www.modk.it/" rel="nofollow">Modkit</a> and our <a href="https://learn.sparkfun.com/curriculum/25" rel="nofollow">Reprogramming Simon</a> material.</p></p>
Greggor on Scratch Programming with the PicoBoardGreggorurn:uuid:a6308fce-4bc2-ea34-d640-102a01316e652013-04-30T11:31:57-06:00<p>There wont be any streaming, but I'll be there taking plenty of video of the ceremony. Look for it in a few days.</p>
co_buckfast on Scratch Programming with the PicoBoardco_buckfasturn:uuid:c613e1de-23dc-edf8-b622-1d696d21036b2013-04-30T11:27:20-06:00<p>Can the Simon board be used as an input to Scratch? Since children might often be introduced to electronics through the Simon game as a soldering project and it has the programming header, it would be neat to repurpose the board as an analog/digital input/output for Scratch. Anyone know how to do this?</p>
sgrace on Scratch Programming with the PicoBoardsgraceurn:uuid:b14f9cb6-bbee-12fd-4be4-241e7f1e73e02013-04-30T10:50:39-06:00<ol>
<li>Congrats on the ground breaking of the new building! Too bad you guys can't stream it.</li>
<li>If only Scratch would work on HDL code... It would make teaching FPGA/CPLDs so much easier.</li>
</ol>