SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T11:53:43-06:00SparkFun ElectronicsBlackJester on SparkFun Eagle Library UpdateBlackJesterurn:uuid:81b128b8-a576-d934-5339-5cc868266fb52011-02-22T11:35:54-07:00<p>Just thought I'd let you know that the +/- pins on the JST-2-SMD are backwards. Also, the USB-MICROB Symbol isn't being used for a USB-MICROB device. There are no devices that use MicroB with both the ID and Shield. Otherwise, always appreciate the library updates. Thanks!</p>