SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T01:30:51-06:00SparkFun Electronicspheinrich on Remake Remodelpheinrichurn:uuid:57a6b222-7618-a279-4e59-b597cbbb8c5d2008-07-07T13:48:56-06:00<p>The 74HC4050D is also handy. It's a hex buffer that runs on as little as 2V while accepting up to 15V inputs. Propagation delay depends on operating temp and VCC, but it has no trouble interfacing a 3.3V SPI flash memory to a 5V PIC at 24MHz.</p>
Nate on Remake RemodelNateurn:uuid:49a04760-326c-4201-5866-699019b719082008-06-23T11:01:15-06:00<p>Nice find! Great looking part if you need single channel.</p>
niwnfyc on Remake Remodelniwnfycurn:uuid:877e47e4-e184-7537-5759-653b143a0afd2008-06-20T09:56:15-06:00<p>Another option for level conversion is this 6-pin IC:<br>
SN74LVC1T45DBVR<br>
$0.59 on mouser</p>
Dpat on Remake RemodelDpaturn:uuid:248bfd88-9795-3f48-ae38-18cd2288db9a2008-06-20T01:50:44-06:00<p>Uber board is excellent learning opportunity to play with GPS,Bluetooth and come up with some nice design . you guys are amazing keep up good work !</p>