SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T05:33:31-06:00SparkFun ElectronicsSarah Al-Mutlaq on T³: Connected Chess BoardsSarah Al-Mutlaqurn:uuid:24a3a169-2dee-3393-0613-56e0ae1ff38f2016-08-03T10:47:11-06:00<p>It would tell you that too many pieces are taken off the board, and to put them back the way they were befoe you can take your official move.</p>
Patrick3coffee on T³: Connected Chess BoardsPatrick3coffeeurn:uuid:c14dd46d-e62a-586a-be0b-3ee200d15d912016-08-03T08:18:19-06:00<p>what happens if the board gets bumped and several pieces fall over? Does it send to phant the first "move" detected and ignore the rest?</p>
RBERLIA on T³: Connected Chess BoardsRBERLIAurn:uuid:958ca39a-adc9-ec2a-ab6c-66860596bf8a2016-08-02T23:46:32-06:00<p>This is awesome! :)</p>
Eric15 on T³: Connected Chess BoardsEric15urn:uuid:e14d45a8-c2d1-611c-b743-324c46dbcab22016-08-02T13:48:27-06:00<p>Neat project, but the $890 price tag for just the electronics exceeds my lifetime chess board budget.</p>
Sarah Al-Mutlaq on T³: Connected Chess BoardsSarah Al-Mutlaqurn:uuid:10f57c30-eff0-7e76-8533-2734e8f4a6a82016-08-02T11:58:08-06:00<p>This (https://data.sparkfun.com/streams/2JYaxdVrEbsrL8maXZJL) was the stream I was using, but it was also for testing and stuff, so you're not going to see a full game on there.</p>
ME heat o nator on T³: Connected Chess BoardsME heat o natorurn:uuid:8ec82a8f-cefd-8474-5d50-3cbf4b293eb82016-08-02T11:29:51-06:00<p>What is the address to see the data from an actual game?</p>
Sarah Al-Mutlaq on T³: Connected Chess BoardsSarah Al-Mutlaqurn:uuid:acf932ae-7f4f-f0f7-fbc7-954f2783aeb62016-08-02T10:39:51-06:00<p>You are correct, it is Phant.io or data.sparkfun.com if you are going to be posting stuff to it. I have fixed it, Thanks! ^_^</p>
ME heat o nator on T³: Connected Chess BoardsME heat o natorurn:uuid:c5108e54-ede3-8f3b-770f-103595694f4c2016-08-02T10:32:12-06:00<p>your phant link doesn't seem to work.</p>