SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T06:50:55-06:00SparkFun ElectronicsCustomer #134773 on Friday Product Post: The Golden AudioCustomer #134773urn:uuid:51bd56b8-e359-3487-d5cd-002d99b473d12019-08-02T14:56:09-06:00<p>For quite a few hours (about 2 days, in fact) I was getting the "we're putting ourselves back together" thing instead of the usual SparkFun web site. The thought occurred to me that if someone were "desparate" to order something, they could (likely) call up and place an order by telephone -- IM[NS]HO, it would be wise to modify the "back together" page to include said telephone... (Fortunately, I didn't happen to need to order anything at the moment, and could probably dig up the number from other resources.)</p>
One Chris Two Chris Red Chris Blue Chris on Friday Product Post: The Golden AudioOne Chris Two Chris Red Chris Blue Chrisurn:uuid:378e176b-7bc6-dc73-a20f-3f6d5e6d75542019-08-02T10:14:46-06:00<p>Yup, totally a typo. It should be "prevent" rather than "provide," I believe.<p>Thanks for the catch!</p></p>
knuckles904 on Friday Product Post: The Golden Audioknuckles904urn:uuid:4b5efc56-9b29-dcec-e666-5fcb578c19842019-08-02T10:05:48-06:00<p>Is this a typo? "This version of the sensor has additional control circuitry that can provide inconsistent "bouncy" data depending on the application."<p>If its not a typo, then I would prefer you keep that additional circuitry and I'll go about my day without inconsistent bouncy data. ;-)</p></p>