SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T23:53:59-06:00SparkFun Electronicsjoe555 on Rock Bottom Powerjoe555urn:uuid:852f6149-94cc-c719-2b18-ae7190a40a412011-08-23T16:55:00-06:00<p>Idle current is one of the important factors in low power design. However, there are more factors including:<br>
1. How long does it take to change from idle to active in order to do something useful? It will impact the overall budget and if it is too slow, it may cause you to miss the event.<br>
2. What is the active mode current? Even for low duty cycle, it has an overall impact.<br>
3. Can it do something useful at low power mode? e.g. DMA capture.<br>
TI MSP430 and Microchip PIC XLP series are very good and metioned. There is a newcomer, EnergyMicro EFM, worths taking a look. 0.9uA draw, with 32KHZ osc on, brown out detector enable, and memory data retention.</p>
Promptcritical on Rock Bottom PowerPromptcriticalurn:uuid:9ac8338f-e1fd-e607-463f-ae16fc5f25652011-08-19T20:29:07-06:00<p>For $6 you can get an energy harvesting chip, hook it ti a TEG or a pezio and not worry and about micro amp sleep modes.</p>
Sparko4Marko on Rock Bottom PowerSparko4Markourn:uuid:c6f88984-fde2-f990-1bf3-d29d3815f1352011-08-17T18:36:57-06:00<p>A shameless plug...<br>
You can build your own ISP, for this project and other Atmel chips. Tutorial link below.<br>
https://sites.google.com/site/projectstruix/projects/isp</p>
noworries on Rock Bottom Powernoworriesurn:uuid:629185f7-f69a-8760-95bd-88b02306df622011-08-17T16:45:04-06:00<p>Yes, air is a better insulator than a PCB, but it is seldom that one needs to resort to such extreme measures as the cost of a production run with such techniques used would likely be prohibitive.<br>
I have used the technique Bob suggested on both DIP and SOIC parts in the past for very high impedance / low leakage circuits which works well for small production runs.<br>
It is sad that Bob is no longer with us, he will be missed.</p>
TheRegnirps on Rock Bottom PowerTheRegnirpsurn:uuid:c225a615-1cc8-5bbd-5dfb-dbdcc50777232011-08-17T16:02:53-06:00<p>As long as it is a DIP part, you can do even better with no PCB and something like Kynar wire-wrap wire soldered to the pins of various parts. Ball it up when finished for super light weight and lowest possible leakage. Here is a Bob Pease circuit.<br>
http://www.rfcafe.com/references/electrical/bob-pease-breadboard.htm<br>
Ooooh! Linear 1 and Linear 2! Along with National's "Linear Applications", they are an education in themselves. If you can find an old copy of the Linear Applications data book, get it by hook or by crook.</p>
sgrace on Rock Bottom Powersgraceurn:uuid:dbb22497-f284-ea05-b899-6e5042d8b6ff2011-08-17T16:02:45-06:00<p>If you've watched EEVBlog, you might know that the creator David Jones made a project to measure that low with good accuracy.<br>
It's called the <a href="http://www.alternatezone.com/electronics/ucurrent/" rel="nofollow">uCurrent</a>. I would check it out.<br>
The DMMs that Nate is using, not sure on the accuracy, but the uCurrent would be a good device to use to check.</p>
Q_tipped on Rock Bottom PowerQ_tippedurn:uuid:baf4a1b4-9f1d-a355-3c6f-d92d3a854ee62011-08-17T15:55:56-06:00<p>Is it just my browser, or is the article date really saying it's the 18th? Last I checked, today is the 17th.</p>
mkings01 on Rock Bottom Powermkings01urn:uuid:daf111b4-7d3a-80b0-e6a1-d561461b96122011-08-17T15:37:38-06:00<p>Yes you can. KCL.</p>
mkings01 on Rock Bottom Powermkings01urn:uuid:92bd3d12-43d5-a877-c719-0157d3331f6e2011-08-17T15:37:29-06:00<p>Thanks to KCL, the only thing you need to worry about in this case is current leakage through other paths, and that will be negligible. 1uA is a good measurement.</p>
mkings01 on Rock Bottom Powermkings01urn:uuid:9cb739e9-f2d8-3ecf-7b9d-350309e5cdce2011-08-17T15:36:52-06:00<p>what this 8MIPS power house sips for power... while running at 0 IPS.<br>
1uA sounds low, but any modern micro-controller worth its salt can do it.</p>
IllogicGate on Rock Bottom PowerIllogicGateurn:uuid:d3ae8544-d327-a249-dc8f-4ccecb2209832011-08-17T15:29:02-06:00<p>It is now.</p>
SomeGuy123 on Rock Bottom PowerSomeGuy123urn:uuid:ad64636f-f4db-677b-6a3d-e55e2591d70f2011-08-17T14:19:14-06:00<p>I thought that as well until I saw <a href="http://sfecdn.s3.amazonaws.com/tutorialimages/PowerAdventures/PowerAdventure-5-M.jpg" rel="nofollow">this picture</a>.</p>
noworries on Rock Bottom Powernoworriesurn:uuid:85acc16f-5715-7107-2f97-19f0e5c18a542011-08-17T14:07:15-06:00<p>Another note regarding low power microcontrollers is to avoid the temptation of setting unused GPIO lines as inputs without tying them either high or low. While it may seem to allow for lower current consumption on the bench, later on some leakage current may cause a GPIO line to float to a voltage that is halfway between a high and a low, where the current that will result internal to the microcontroller will be several milliamps.<br>
Setting an unused pin as an input with an internal weak pullup is probably your best bet, but don't be tempted to leave them floating without a pull up or pull down resistor be it internal or external.</p>
noworries on Rock Bottom Powernoworriesurn:uuid:c8547dad-1950-2ff4-6c3c-45aea9790ea42011-08-17T13:57:04-06:00<p>You may even be able to get slightly less current consumption if you do away with the breadboard and are careful to keep the components clean and dry. If you do the math, 1uA at 3.3 volts is an equivalent resistance of 3.3 Megohms. Breadboards that have been used a while can be pretty leaky, a clean epoxy PCB is better. Do clean the flux off, however. Also, you may want to consider a low leakage conformal coating for the components and printed circuit board if you desire the current consumption to be kept low for long durations (months - years). This is because leakage that may occur due to humidity and PCB board contamination over time may become significant sources of power loss for your battery.</p>
Kilo on Rock Bottom PowerKilourn:uuid:a0368410-7122-5c74-5bcd-66d6f66c563c2011-08-17T12:19:26-06:00<p>Imagine the measurement uncertainty at that lo range on a hand meter without kelvins..+/- 30%?</p>
BlackJester on Rock Bottom PowerBlackJesterurn:uuid:b8ca4476-a4c2-011e-7672-041a5adc02c22011-08-17T11:25:04-06:00<p>BREAKIN' THA LAW! BREAKIN' THA LAW!</p>
BlackJester on Rock Bottom PowerBlackJesterurn:uuid:7ff82593-3d49-9e96-5916-8d53286f8c642011-08-17T11:23:44-06:00<p>I think that's an ESD mat.</p>
TeslaFan on Rock Bottom PowerTeslaFanurn:uuid:3c6f9e8f-9007-47f1-1731-bfe080a1ed712011-08-17T10:02:17-06:00<p>Can you even legally measure down that far with that set up? I think those jumpers alone need more than that to stay up!</p>
48X24X48X on Rock Bottom Power48X24X48Xurn:uuid:9c824003-b3c7-e356-0f28-ba0129d3513f2011-08-17T10:01:24-06:00<p>You guys might want to try an Arduino compatible low power library that we wrote: https://github.com/rocketscream/Low-Power<br>
if you don't want to mess around with the fuses.</p>
SomeGuy123 on Rock Bottom PowerSomeGuy123urn:uuid:cd8b7ef6-b315-5d7a-33e9-cadc6e5dab082011-08-17T09:36:37-06:00<p>Is that a Sparkfun mouse pad I see on the far right of the picture?</p>
Kamiquasi on Rock Bottom PowerKamiquasiurn:uuid:f9d54a36-257a-a7a1-7ad3-1529d5fe0a152011-08-17T09:29:38-06:00<p>how 'bout now?</p>
IllogicGate on Rock Bottom PowerIllogicGateurn:uuid:6b919733-d2ac-ff71-ea8e-a313f95be3ac2011-08-17T09:28:12-06:00<p>Hmm. This article isn't showing up in Google Reader OR iGoogle.</p>