SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T07:09:13-06:00SparkFun ElectronicsCustomer #461783 on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUCustomer #461783urn:uuid:02a17b17-4346-9ea1-fa5d-6cdf332ad6242013-08-14T10:39:27-06:00<p>Sir, I also want develop a similar project as you have stated ie. a UAV or an autonomous plane.... I have good command on c programming of atmega controllers . I'm new in world of arduino but found it quite easy . So surely would be using arduino for my project . I have a idea of how can I put a autonomous system into a plane . But I need help .... Sir , please give me whatever information you have ie. code snippets ,algorithms, equtions anything .... I will be very thankful to you</p>
A. Babb on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUA. Babburn:uuid:ddb5844a-1adb-b5d8-195e-28be55bf3be42011-07-20T08:50:28-06:00<p>Out of curiosity, what is the reccomended samping rate for this board?<br>
From looking at the schematic (and referring to the supplied datasheets), I see that the Gyro's have a -3dB LPF at around 48Hz and the Accelerometers have a -3dB LPF at 50Hz.<br>
I'm currently running the ADC at a rate of 110Hz, and I'm worried that I might be sapping some performance and/or introducing noise...</p>
A. Babb on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUA. Babburn:uuid:4aef0207-b487-7063-96a4-8b78b339ad882011-06-29T16:29:35-06:00<p>It's one of several different coordinate schemes:<br>
This board has the X and Y angle set up so that a positive X angle tilt will result in a positive linear acceleration (and displacement) along the X axis, and a positive Y angle tilt will result in a positive acceration along the Y axis.<br>
It seems like this was more intended for quadrotors and helicopters than for airplanes and other craft.</p>
Jesse214 on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUJesse214urn:uuid:016a3d18-34f1-cf48-d80c-b6748951af462011-06-13T21:06:19-06:00<p>From the schematic, the V1 and V2 pins are VREF's for the gyro chips. I don't use these, and the data sheet indicates to use the VREF's if using only the non-amplified outputs.<br>
As for what pins to use, use the 3.3V pin for power. Use the GND pin for ground. I also use the Gx4 gyro pins and the accelerometer pins next to those. I don't use any pins on the other side of the board.</p>
Jesse214 on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUJesse214urn:uuid:155f83bc-e0f6-726c-1fa3-9d99e4a23d602011-06-11T21:59:20-06:00<p>Great board! I'm using it to develop my own UAV. I've posted Arduino code for fusing the data and displaying it on an attitude indicator program, which I also made(its available for download). All can be found <a href="http://www.nuclearprojects.com/imu" rel="nofollow">HERE</a>.</p>
riggosf on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUriggosfurn:uuid:671189e0-6a5c-4632-0fe7-1caa1b5f671e2011-06-11T16:18:05-06:00<p>I have a couple of questions about the pins:<br>
- why are there two voltage pins? V1 and V2<br>
- What is the 3.3V pin for and what should it be connected to<br>
what input current can be safely given to the IMU?</p>
Customer #117242 on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUCustomer #117242urn:uuid:4a840509-30f1-c3e5-0c9c-47fe514064742011-05-19T03:37:11-06:00<p>Yes, I dont get anything useful out of it either in the Z. Also, Im guessing no-one has tried with a Li-Poly battery as these are 3.7v which is likely too much. Maybe a diode would help there?</p>
Lauszus on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMULauszusurn:uuid:b769ec44-c278-5c15-9477-bbf428df67892011-04-10T17:25:40-06:00<p>Check my guide out. It is based on this IMU: <a href="http://arduino.cc/forum/index.php/topic,58048.msg417140.html#msg417140" rel="nofollow">Guide to gyro and accelerometer with Arduino including Kalman filtering</a></p>
Lauszus on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMULauszusurn:uuid:1b0bc3e7-4321-18fc-4d5f-ded9084a8b2e2011-04-09T13:40:57-06:00<p>I made a guide on how to use this IMU with the Arduino including a Kalman filter:<br>
<a href="http://arduino.cc/forum/index.php/topic,58048.msg417140.html#msg417140" rel="nofollow">Guide to gyro and accelerometer with Arduino including Kalman filtering</a></p>
fz on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUfzurn:uuid:e49e33e4-df0a-b37d-2ed9-c8c38b0c37512011-03-18T17:40:13-06:00<p>Has anyone encountered problems with z-axis gyro reading? For some reason when I connect to the 4x output, the stationary reading oscillates at 1.2 +/- 0.1 V at 87Hz (sensitivity is only 3.33mV/deg, so I'm reading crazy values), while x and y readings are perfectly accurate.</p>
Customer #210093 on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUCustomer #210093urn:uuid:7596e442-9522-1dd4-4ebf-851044a85b5f2011-03-13T13:04:50-06:00<p>can anyone tell me how im able to interface the gyros with the accelerometers in this board??<br>
im trying to make an inertial navigation system by connecting this board with an arduino and im really lost. could really do with some help!</p>
GearJammer on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUGearJammerurn:uuid:441924b4-b0b2-7322-8b4c-a472d48ca3a62011-02-26T16:31:55-07:00<p>All Gyros exhibit this behavior. It's called gyro drift. You have to calibrate it out. Also the drift will vary over temperature. The big downside I see to this IMU is no temperature readings. You may test your quadrotor inside and everything is fine. then take it outside in the Hot or Cold and it will behave differently because the sensor reading will vary some based on temperature.</p>
jesgatt on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUjesgatturn:uuid:67546195-3825-2a14-fdff-5812d5e5c1292011-02-09T09:35:05-07:00<p>@ Racine : Hi, any help re how to integrate (Kalman filter) for a quad rotor. Apart from that, the Z-axis value is not similar to the X and Y since it is +30 more than the latter</p>
Niz on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUNizurn:uuid:e3a637a4-f9f1-8c4f-9176-7b3ebe4d56442011-01-25T17:33:58-07:00<p>Hi, I have a 1"x 1" small PCB that does 6 degrees of freedom on batch PCB.<br>
http://batchpcb.com/index.php/Products/51805<br>
I2C interface</p>
theredrook on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUtheredrookurn:uuid:0e6774ae-0fac-96fa-1da2-87dbcf2a94652010-12-29T09:21:06-07:00<p>is this compatible with xbee or zigbee or any other wireless like bluetooth? if not please tell me a good imu + wireless solution!<br>
is razor 9 dof + bluetooth mate ok?<br>
i need to make a 3d mouse pointing device using that!<br>
please help thanks.</p>
Jaspal Singh on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUJaspal Singhurn:uuid:3e8a9e37-0d37-9443-b75b-c42629973e0c2010-10-29T12:36:31-06:00<p>How come this board doesn't align the x and y axis on each sensor? From the readings, you could program the micro controller accordingly, but it seems better if the X and Y were aligned.</p>
johndavid400 on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUjohndavid400urn:uuid:ab9ac49c-4270-370a-7100-b712898f44d62010-10-13T00:04:43-06:00<p>Works well for angular positioning, but the gyros idle a bit lower than the accelerometer... when reading these from my Arduino via the 10-bit Analog inputs (with Aref tied to 3.3v), the accelerometer outputs centered right at 512 when "level" (scale of 0-1023) - while the gyro outputs all centered around 390 (when sitting still)? I thought this was a bit odd, but it is also stated in the datasheet that center voltage for gyros is 1.23v.<br>
By combining the X outputs from both accel and gyro to my Arduino, I made a weighted complementary filter to control a Segway type ridable bot. It works great!</p>
aplejuce on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUaplejuceurn:uuid:d53820a1-fb45-a906-98ea-ca0aa248c56c2010-09-16T12:05:25-06:00<p>Perfect! thanks! Just ordered one!<br>
~long live the sparkfun</p>
anfedres on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUanfedresurn:uuid:a5f780bb-7f17-28a7-2bff-cfb2cdd20ef32010-09-14T11:41:59-06:00<p>Analog my friend.</p>
anfedres on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUanfedresurn:uuid:d293d37e-cba6-0632-5137-58b3c4a9d9042010-09-14T11:40:32-06:00<p>Someone has problem with the Gyros, or it's just me, I can't integrate the speed to obtain the position.</p>
aplejuce on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUaplejuceurn:uuid:3caf7a07-3754-124c-cf43-0a27d0c4bba72010-09-12T10:33:13-06:00<p>What is the output of this board? analog or digital signals?<br>
thanks</p>
anfedres on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUanfedresurn:uuid:ffa70105-845e-d541-9627-c0a84a7d2bc82010-08-29T12:19:48-06:00<p>Has Anyone tried this IMU?</p>
Racine on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMURacineurn:uuid:d2dcb697-34f3-1d63-6cc2-38b1a79b870e2010-08-25T05:19:34-06:00<p>Hi!<br>
He's not bad for quadrotor, but you must use Kalman filter for coupling accelerometer output with gyro output. And be carefull with the number of output, because he ask 6 analog input for reading, maybe we don't have enought free on your board coupling with other sensors, for example adding magneto ...</p>
anfedres on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUanfedresurn:uuid:bc8b809c-3428-1825-4541-c58010a4875a2010-08-22T20:15:26-06:00<p>What do you think about this IMU in a Quadrotor???</p>
cyberfish on SEN-10010 - IMU Analog Combo Board Razor - 6DOF Ultra-Thin IMUcyberfishurn:uuid:42cba38d-b1b7-ffeb-9867-e6b6d23354922010-08-07T12:35:30-06:00<p>Is there any reason to go for this one instead of a ITG-3200 breakout + ADXL335 breakout which actually turn out to be slightly cheaper(?!)</p>