SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T07:35:58-06:00SparkFun Electronicshmmmmm on COM-10028 - MEMS Microphone - INMP401 (ADMP401)hmmmmmurn:uuid:f7417803-3fba-53c2-f68e-fee6910c22602014-08-04T11:49:36-06:00<p>I have used many different small speakers to record sound. Has anyone used this mic as a tiny speaker (ear bud or within the ear) or know if it would work?</p>
RobertC. on COM-10028 - MEMS Microphone - INMP401 (ADMP401)RobertC.urn:uuid:d020b73b-03ca-de98-a8e6-11fe6fbe509f2014-04-22T09:34:42-06:00<p>check out page 5 and 6 of the datasheet.</p>
Robocasters on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Robocastersurn:uuid:b9f5bd1d-3ca4-bf0c-5242-67a7515833222014-04-22T01:50:03-06:00<p>For what reasons is there a hole at the bottom. Do we need to connect that to ground. No such ground connection shown for the breakout board.</p>
Customer #302799 on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Customer #302799urn:uuid:af9b30dc-3cb6-29f7-440d-27a6e57c72232013-07-02T08:53:15-06:00<p>Confirmed by the pictures, it is the same size no matter witch way you flip it. :)</p>
Customer #431947 on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Customer #431947urn:uuid:65ca5b33-991d-1e39-7c5d-1e266fc7c6662013-04-24T02:28:52-06:00<p>sir i require an MEMS sensor
how can i get it</p>
Customer #370606 on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Customer #370606urn:uuid:089d231e-85d5-7379-00d9-5134cf0ab8692012-10-17T07:14:57-06:00<p>add a via in the footprint, heat it from the other side of the PCB with the soldering iron.</p>
Customer #345123 on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Customer #345123urn:uuid:863f1eaa-7073-7d51-47b9-26abe708905b2012-08-11T06:35:54-06:00<p>Wonder if this would be suitable for a bat listener?
the small size of the MEMS should make it ideal methinks.<p>-A</p></p>
ATtiny Fan on COM-10028 - MEMS Microphone - INMP401 (ADMP401)ATtiny Fanurn:uuid:95a8dd91-902a-34ec-5bb7-40c56642314d2012-06-04T18:26:57-06:00<p>Magic fairies that crawl under it and explode to heat up the pads.</p>
Customer #91088 on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Customer #91088urn:uuid:46e1542b-7686-6e7a-2d10-6d845b012b572011-11-15T08:07:39-07:00<p>What is the best way to solder it?</p>
Bret Mattingly on COM-10028 - MEMS Microphone - INMP401 (ADMP401)Bret Mattinglyurn:uuid:133755e4-fd59-f4c4-7c58-585e5e9be0db2010-07-22T09:36:49-06:00<p>LMFAO!<br>
"We are working on a breakout board and will have it available shortly after you actually needed it."<br>
Score one for honest businesses haha. You guys are great.</p>