SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T07:33:47-06:00SparkFun ElectronicsCustomer #406887 on ROB-10077 - Wheel 90x10mm Pair - BlackCustomer #406887urn:uuid:f011707d-b265-9f0e-2a97-bda63caa5e5c2013-03-15T21:45:51-06:00<p>Does anybody know where I can find just a 3mm shaft? I want to use a set of these for non drive wheels but I'm not sure the best way to mount them if not connected to a motor.</p>
Customer #406887 on ROB-10077 - Wheel 90x10mm Pair - BlackCustomer #406887urn:uuid:2730e4d6-af09-8a19-b809-9ed64a43148e2013-03-15T21:35:01-06:00<p>I just mounted servos to mine with the supplied screws and the star hub and it was a cinch.</p>
Customer #327198 on ROB-10077 - Wheel 90x10mm Pair - BlackCustomer #327198urn:uuid:1924e17e-5bb8-a964-aa4a-53e283daf7832012-05-27T22:34:36-06:00<p>Will these work with your hobby motor you must answer just kidding please though</p>
Ben9 on ROB-10077 - Wheel 90x10mm Pair - BlackBen9urn:uuid:9f2d6b95-d3ce-cb84-26fc-d42f3bdae2ad2011-08-10T10:56:08-06:00<p>These wheels have mounting holes that work with Pololu's <a href="http://www.pololu.com/catalog/product/1083" rel="nofollow">universal mounting hub for 6mm shafts</a>, which makes it easy to use these wheels with Pololu's 37D mm motors (the wheels also work with the 4mm and 5mm mounting hubs if you want to use them with other motors).</p>
SomeGuy123 on ROB-10077 - Wheel 90x10mm Pair - BlackSomeGuy123urn:uuid:8e48e779-f63b-45d9-5497-7bc022435e5a2011-07-14T14:50:20-06:00<p>37D shafts are 6mm. This wheel is designed for 3mm shafts.</p>
kuzyt on ROB-10077 - Wheel 90x10mm Pair - Blackkuzyturn:uuid:20b73f5a-32c4-2c54-f44a-0a5cef9c64762011-07-13T20:41:39-06:00<p>hey do these work with 37D mm motor shafts ?</p>
SomeGuy123 on ROB-10077 - Wheel 90x10mm Pair - BlackSomeGuy123urn:uuid:636310d3-0e31-f618-02f8-97ecb65020442010-12-20T19:50:20-07:00<p>The spacing is a bit off.</p>
RobertC. on ROB-10077 - Wheel 90x10mm Pair - BlackRobertC.urn:uuid:b2570638-4a20-07de-86ae-ce6e4d4ffd6b2010-10-19T09:57:48-06:00<p>Use one of the hubs that come with the servo and then just screw it together. It works fine because the screw spacing is the same on the wheel as in the servo hubs.</p>
SomeGuy123 on ROB-10077 - Wheel 90x10mm Pair - BlackSomeGuy123urn:uuid:5211e16e-503b-bdcb-9e0c-6b7244afd2432010-10-18T21:16:18-06:00<p>I bought these from a different site, but I just wanted to say that these are a pain to attach to servos (modified for 360 deg.) I ended up using some double sided foam tape from servocity to attach them to the servo hubs. Hot glue would probably work as well.</p>