SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T06:25:54-06:00SparkFun Electronicstrodoss on KIT-10226 - Video Game Shieldtrodossurn:uuid:90f50426-54d3-ed0e-636b-429198e7497c2012-07-23T09:56:31-06:00<p>Another really cool example that is a little hard to find on the Wayne and Layne site is a Raycaster engine that they wrote: <a href="http://www.wayneandlayne.com/forum/viewtopic.php?f=11&t=107" rel="nofollow">Forum Post</a><p>Thought I would pass that along.</p></p>
trodoss on KIT-10226 - Video Game Shieldtrodossurn:uuid:e81fcf65-3179-0303-1977-7bd7a800ec862012-06-20T12:00:42-06:00<p>Glad you like the projects!
For those who haven't seen it, video for Elventure is here:
<a href="http://www.youtube.com/watch?v=P6qI4Rs3WU0&feature=player_embedded" rel="nofollow">YouTube Video of Elventure</a><p>The video is from the Hackvision version, but both the Video Game Shield and Hackvision versions are functionally the same.</p></p>
jago lee on KIT-10226 - Video Game Shieldjago leeurn:uuid:b0376adf-59b1-7d90-2033-13cb1ebf35af2012-06-07T03:15:49-06:00<p>WOW! Thanks for sharing your ingenuity with me. That's a great video too! Looking forward to seeing more.</p>
jago lee on KIT-10226 - Video Game Shieldjago leeurn:uuid:6282d494-56b0-0eb1-4e59-7784f0646cd42012-05-31T09:34:39-06:00<p>Ok, theres many things that could be wrong with your board. Firstly the arduino will tell you if your code is wrong. If so use a diferent code. Secondly check for cold joints, solder bridges, ETC. Thirdly, if your multimeter has a continuity setting on it check for breaks in the circuit. I hope this works :) if not email me at jagolee@hotmail.co.uk.</p>
ChadWV on KIT-10226 - Video Game ShieldChadWVurn:uuid:c074a4da-7ffa-9f1c-1a77-16e32a0058f92012-05-12T08:57:38-06:00<p>I just built the game shield, but none of the code works for me. I tried the sample stuff from Wayne and layne nothing but errors can someone help ?</p>
joeyxl on KIT-10226 - Video Game Shieldjoeyxlurn:uuid:669b0c6c-9be3-4346-8b28-3868d1631a902012-01-13T01:07:07-07:00<p>yes spark fun would never give out somthing that does not work its is tested by the the top people in sparkfujn the best from all over the world and evean if they did put it out the would take it back and give you a full refund.</p>
trodoss on KIT-10226 - Video Game Shieldtrodossurn:uuid:c6189891-3089-7e9e-1122-326421a1b4502012-01-12T14:34:06-07:00<p>I agree, it definitely works!<br>
I have used it on a few projects, see: <a href="http://code.google.com/p/trodoss-arduino/" rel="nofollow">http://code.google.com/p/trodoss-arduino/</a></p>
jago lee on KIT-10226 - Video Game Shieldjago leeurn:uuid:749612f8-42c5-61b4-4336-6f9c163f953f2012-01-10T09:20:18-07:00<p>chiel its a add on to Arduino, you add it to what ever one you have like a arduino uno. trust me this kit works!</p>
MoriFi on KIT-10226 - Video Game ShieldMoriFiurn:uuid:679a03b7-884d-e7f1-a181-02b116af0cf92011-06-05T13:51:24-06:00<p>color runs at a higher frequency to. I forget what it is though.</p>
A.G. on KIT-10226 - Video Game ShieldA.G.urn:uuid:8018cd98-d600-55b4-0e05-5943b37f82c92011-04-16T11:20:20-06:00<p>I was wondering if there a way/hack available where I can convert the composite video to VGA so that I can view the shield's output on a monitor? This would be helpful to demo a game I am working on.<br>
Thanks!</p>
wayne_and_layne on KIT-10226 - Video Game Shieldwayne_and_layneurn:uuid:4cf94386-cb40-3b16-3058-4bf507c7f87d2011-04-12T08:13:44-06:00<p>We're working to get a Netduino and set up the windows environment to start working on it. I'll let you know when we have it working with the Netduino. Might take a few weeks to get it working.</p>
Mr. Person on KIT-10226 - Video Game ShieldMr. Personurn:uuid:2b02ec3b-54ea-af5d-b835-86d763d60ccb2011-02-05T06:55:13-07:00<p>Wait, would color be possible using a more powerful board, like the Netduino or FEZ Panda?</p>
Ivan747 on KIT-10226 - Video Game ShieldIvan747urn:uuid:52a7d516-a738-049c-6819-4ff3773f18462011-01-27T15:11:08-07:00<p>A supporting NTSC and two Wii nunchucks makes me wonder how much can you do on an AtMega328 running a bootloader.</p>
Mr. Person on KIT-10226 - Video Game ShieldMr. Personurn:uuid:10ff1ff2-2e04-0f15-98a7-26956e7167552011-01-08T09:21:29-07:00<p>Thanks for the help.</p>
Mr. Person on KIT-10226 - Video Game ShieldMr. Personurn:uuid:83942271-6617-8b89-2a34-3a308514f6932011-01-08T09:20:50-07:00<p>Is there any chance of a .NET Micro Library coming out for this shield?</p>
wayne_and_layne on KIT-10226 - Video Game Shieldwayne_and_layneurn:uuid:bbd4e504-f7c7-6462-a744-5004e36ed9c52011-01-02T15:46:12-07:00<p>I don't think that changing the colors, even staying with only two colors, would be possible with the current hardware. If you change the values of the resistors for video and sync, you might be able to have black and gray, or gray and white, or something like that, but color would be trickier, I think.<br>
The tellymate shield doesn't include the nice connectors for the Wii accessories (Nunchuck, Classic Controller, etc), but it only uses the two serial pins for the arduino to talk to the tellymate chip. The tellymate chip handles all the tricky business of generating the video signal, which is all done by the arduino with the video game shield. The tellymate looks like it's all text-based, although they can deal with individual pixels by using a special font, where each character is some combination of lit/unlit pixels. Also, the tellymate is a little more expensive than the video game shield.</p>
Mr. Person on KIT-10226 - Video Game ShieldMr. Personurn:uuid:8f1854b6-1e02-e748-a5c8-17355211b1e32010-12-11T20:55:05-07:00<p>I am wondering, can the colors be changed besides black and white? I mean, there would still only be two different colors, but the two would be different from black and white.<br /><br>
<br /><br>
Also, how does this compare to the Tellymate Shield? Is it better? Is it worse? Is it about the same?</p>
wayne_and_layne on KIT-10226 - Video Game Shieldwayne_and_layneurn:uuid:5f5d587b-2810-9496-8524-aecbfdeb261c2010-12-08T08:53:24-07:00<p>Thanks! Glad you like the Video Game Shield. We've just added support for the Wii Classic Controller, in addition to the Nunchucks, and are planning to release a new library that supports the Wii Motion Plus rotation sensor module.<br /><br>
<br /><br>
You're very right about the Wii accessories sharing the same address: Most of the hardware on the Video Game Shield is involved in supporting the two controllers at once, doing the switching and level-conversion between 5v and 3.3v.<br /><br>
<br /><br>
You can indeed just plug in the controllers, as we have some specially designed cutouts on the circuit board.</p>
Ted M on KIT-10226 - Video Game ShieldTed Murn:uuid:05ffd82a-f3a4-be7b-0f87-40c330ee09412010-12-07T22:38:02-07:00<p>The cool thing about this is that it puts together audio, video, and two wii controllers on one shield. (Two wii nunchucks are tricky because they all use the same address, so you need a circuit to switch between the wii's) It also looks like it has two connectors for the wii's, so you can just plug them in. Very Cool!</p>
BricoGeek on KIT-10226 - Video Game ShieldBricoGeekurn:uuid:eaea9e36-deca-4acb-eb28-8f9670bf05062010-12-07T08:42:52-07:00<p>here is:<br /><br>
http://www.youtube.com/watch?v=fS9ff2oioew</p>
EvilTwin on KIT-10226 - Video Game ShieldEvilTwinurn:uuid:6206cca9-b139-57a8-2ae0-b718af0937a72010-12-06T19:38:18-07:00<p>I would love to see a you tube clip of this in action.</p>
wayne_and_layne on KIT-10226 - Video Game Shieldwayne_and_layneurn:uuid:b4541e33-0b2b-529e-d700-74858b67a2f82010-12-06T18:42:39-07:00<p>Hello Chiel,<br /><br>
<br /><br>
We have schematics posted on the Download page, located here: http://www.wayneandlayne.com/projects/video-game-shield/download/#hwdes<br /><br>
<br /><br>
We initially developed the circuits on a breadboard, so you should have no trouble making it yourself. The transistors and 4066 IC are used for interfacing with the Nunchucks, so you shouldn't need them unless you are using Nunchucks. The TV-out part is just the four resistors near the top of the board.</p>
Chiel on KIT-10226 - Video Game ShieldChielurn:uuid:77eb8bca-92af-72fb-ffee-c007f1174d502010-12-06T13:23:20-07:00<p>i did not know you could that with some resistors,transistors and a 4066 ic.<br /><br>
<br /><br>
is there a schematic for the circuit? i wouldn't mind trying this out on a breadboard.<br /><br>
<br /><br>
also the tvout examples seem broken. to fix it you just change TV.begin(PAL) to TV.begin(_PAL)(same with the NTSC).</p>