SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T16:37:58-06:00SparkFun Electronicsschlick on DEV-10233 - iPod Connector Male Style 1 - Ding and Dentschlickurn:uuid:10b5a455-318b-e96b-9636-49d7e6eb15412012-04-23T12:35:42-06:00<p>This looks like a QC problem the some one's packaging dept. I bought several and was able to mix-and-match to make complete good connectors. The little spring hooks have part numbers 562-1002 and 562-1003. Some packages had one each, some had two of the same. Probably cost more to repackage them.</p>
Sam R. on DEV-10233 - iPod Connector Male Style 1 - Ding and DentSam R.urn:uuid:09c3b00c-a484-9b93-bf80-12324c90ee822011-02-10T17:46:37-07:00<p>The one that I got was fine....didn't need to do anything to it to get it to work!<br>
Sam</p>
trujillostm on DEV-10233 - iPod Connector Male Style 1 - Ding and Denttrujillostmurn:uuid:27bf885c-37a9-2823-bd74-eec1c1b278ea2010-12-05T09:42:19-07:00<p>Can I file or cut the plastic tab? Only one or two tabs? Can I use it to the iPad?</p>