SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T12:54:40-06:00SparkFun ElectronicsPearce on SEN-10276 - WiTilt v3.0Pearceurn:uuid:a90ee819-3016-f1f9-2760-087364fbf3a72011-09-01T18:23:48-06:00<p>I haven't been able to get it to connect to my phone (Evo 4G).</p>
dds21 on SEN-10276 - WiTilt v3.0dds21urn:uuid:dd5b972f-247d-9901-20e5-12ce6b015fbf2011-09-01T13:40:38-06:00<p>Will the WiTilt pair to an Android device? Are there any off the shelf apps that will allow you to read the serial output from this device on an Android device?</p>
wa7iut on SEN-10276 - WiTilt v3.0wa7iuturn:uuid:dec7a4c0-af1d-b345-ae01-247d3337ff2a2011-07-15T00:35:38-06:00<p>Will the Bluetooth channel and other software support two of these units in operation simultaneously on a single PC?</p>
Snake2 on SEN-10276 - WiTilt v3.0Snake2urn:uuid:61ef8634-cb8e-4808-af98-5161a024d8c32011-03-16T14:28:43-06:00<p>The passcode required to pair to the WiTilt v3.0 is "1234". For the Macbook Pro, here's the steps to get it working:<br>
1. Download ZTerm (Mac equivalent to Hyperterminal)<br>
2. Turn on Witilt<br>
2. click on "Set Up Device" under the bluetooth menu<br>
3. The Witilt is called "Firefly". pair to it using the passcode, then quit. Note that WiTilt is not really connected yet even though it says it is.<br>
4. click on "Open Bluetooth Preferences" under the bluetooth menu.<br>
5. click on the Firefly, and down at the bottom of the menu, right click the settings button and select "edit serial port". The WiTilt connects as soon as you open up this menu.<br>
6. ensure "protocol" is set to RS-232 and "service" is set to SPP. You can also change the "Name" if you'd like (I changed mine to WiTilt)<br>
7. open up ZTerm<br>
8. click "settings", then modem preferences. the name you set in step 6 should be listed as an option in the "serial port" menu. select it as the serial port. clear any "Modem setup strings". click "ok"<br>
9. exit that menu, click "settings", and "connection"<br>
10. for "service name", type the name you set in step 6<br>
11. for data rate select 57600. click ok<br>
12. reset the Witilt, and you should see the main menu come up in ZTerm!</p>