SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-18T20:42:42-06:00SparkFun ElectronicsCustomer #609919 on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerCustomer #609919urn:uuid:1ee29387-b59a-25fc-5d59-7f33f9038f612015-01-21T12:50:27-07:00<p>Same question, i'm interested in buying something like that !
Did you found what you want ?</p>
Inky69 on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerInky69urn:uuid:5a430c55-dc20-4a30-daa1-7e11e54a82bb2014-08-21T06:05:30-06:00<p>I'm having trouble programming this item and since this product is no longer supported at DIY Drones, they don't have any documentation.<br>
1. Does it come with an Arduino bootloader (which one)?
2. Are there mods to a standard Arduino IDE to program it via the TXO-0 and RXI-0 pins?</p>
cphillips on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV Controllercphillipsurn:uuid:b3e94c35-c6a3-8263-abc4-5f57b00784632014-07-17T10:07:30-06:00<p>Please bring this back! The footprint is much smaller than the standard MEGAs and the 0.1" headers are much easier to work with than what the pro Mega mini has. Besides, I have these designed into a few enclosures and now I have to figure out how to get something else in there.</p>
M-Short on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerM-Shorturn:uuid:34f1c9d3-9659-3858-88a3-97d185519d1c2014-07-16T09:16:27-06:00<p>We don't plan on carrying this any more since its a pretty old version. Check out DIYDrones for the current version (2.6 I think).</p>
Customer #500990 on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerCustomer #500990urn:uuid:30f1cfd1-58c9-2009-3d51-4735872296112014-07-16T03:10:33-06:00<p>When it will be avalaible again?</p>
Toni_K on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerToni_Kurn:uuid:87f696ab-82c0-7cc0-4dff-bcd5a171a2022014-05-12T14:09:30-06:00<p>Sorry about that! The receiver had been retired. We've updated to a new product in the links now.</p>
Yosserg on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerYossergurn:uuid:de1bd9dd-c654-4fd1-a4f0-8ca9812481462014-05-12T13:43:33-06:00<p>The "uBlox 5 GPS module and adapter" links in the description are dead links.</p>
Lewma on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerLewmaurn:uuid:91d603e7-b4cb-8a23-c25e-ff677f003bcf2014-01-14T19:58:40-07:00<p>Kind of disappointed that I bought this board then found out it comes with no sensors, and also it's discontinued over at DIY Drones and is no longer supported :(</p>
Customer #336603 on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerCustomer #336603urn:uuid:16506a48-eb23-751f-f14c-61d9f5a3e82e2012-07-08T15:26:21-06:00<p>can I use this as an regular arduino board, without its imu shield?
I am asking because I cant. A simple blink program does not blink the led without the shield on, but it does if the led is connected to the respective pin on the shield. Crazy huh?
Any help?
I want to use it without the Oilpan, as a regular arduino.</p>
brennen on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV Controllerbrennenurn:uuid:8b137279-c279-4820-0310-9074e3343fa12012-05-22T16:17:17-06:00<p>You've had comments deleted before for this kind of thing, but in case it wasn't clear, you're crossing the line into outright spam here. Not cool.</p>
Australian Robotics on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerAustralian Roboticsurn:uuid:e7eedea1-4fb6-ae00-1958-498188f8ff632011-11-03T19:10:21-06:00<p>Will this work with http://www.sparkfun.com/products/465 ?</p>
rwizard on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV Controllerrwizardurn:uuid:6cb7877a-985a-773a-a244-cddf66d357212011-09-12T17:32:05-06:00<p>HungryMaggot,<br>
Don't hold me to this, but I believe that in order to run the 2560 at 3.3 you have to change the crystal from 16 mhz to 8 mhz. Based on a cursory glance at the schematic, I think there is at least one 5 volt only part on the board as well (74LS157D).</p>
rwizard on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV Controllerrwizardurn:uuid:9c7bb237-9e6b-01b7-9fb3-7e9f5542fceb2011-09-03T20:26:31-06:00<p>One more inmate rattling the bars and agitating for the IMU release date.</p>
BazDaddy on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerBazDaddyurn:uuid:d8556587-ca67-4196-4148-a8bd16cba4602011-08-10T00:56:57-06:00<p>Anyone? Anything on this yet?</p>
TQT on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerTQTurn:uuid:681feebd-f267-1843-1e2c-0bb35568dcfd2011-08-08T22:35:10-06:00<p>Yeah, when... with the retirement of the ArduIMU+ we are running out of options to get a full solution from you :)</p>
HungryMaggot on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerHungryMaggoturn:uuid:82128a24-6f07-def9-5ab7-9108314951b72011-07-23T22:22:36-06:00<p>a general question: if it works at 3.3volts will it run at 16 or 8 Mhz</p>
BazDaddy on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerBazDaddyurn:uuid:0123fa37-cc6e-27ea-0e75-4e5aebc67efe2011-07-23T08:05:03-06:00<p>Do you have a date for when the IMU will be available? And will it be the "ArduPilot Mega IMU Shield/OilPan Rev-H V1.0"</p>
BornaE on GPS-10294 - ArduPilot Mega - Arduino Mega compatible UAV ControllerBornaEurn:uuid:b7dba787-37c2-c3df-fd8f-04f52192f8b12011-07-06T13:41:24-06:00<p>"(IMU sensor shield coming soon)"</p>