SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T13:15:25-06:00SparkFun ElectronicsCustomer #842328 on PRT-10474 - XT60 Connectors - Male/Female PairCustomer #842328urn:uuid:48945445-2409-b56f-5822-bef40b84f9e72016-09-09T14:49:17-06:00<p>I was delighted to see the actual drawings of this item. However, there was a dimension left out. Can you reveal the distance between the protruding pins?</p>
RobertC. on PRT-10474 - XT60 Connectors - Male/Female PairRobertC.urn:uuid:3e2ef5be-476e-ccb6-840e-c05b1c8481c72013-07-18T14:47:59-06:00<p>for an immeasurably small amount of time, probably.</p>
Paul Smith on PRT-10474 - XT60 Connectors - Male/Female PairPaul Smithurn:uuid:fbdb500c-697c-d17a-db81-bba9b21630ef2013-07-10T13:03:04-06:00<p>Cool, thanks!</p>
Sleepwalker3 on PRT-10474 - XT60 Connectors - Male/Female PairSleepwalker3urn:uuid:d9cad6a2-0178-13d3-a2c6-6bb679e016fb2013-07-10T12:27:44-06:00<p>Well try this great <a href="http://joshmadison.com/convert-for-windows/" rel="nofollow">conversion program</a>, it's very cool, quick and useful. It's Win anything, but runs on Wine too apparently. I've used it for years and it's really handy and far quicker to use than others I've tried, and it's small enough that it doesn't get in the way :)</p>
Paul Smith on PRT-10474 - XT60 Connectors - Male/Female PairPaul Smithurn:uuid:e82cc645-188d-9f60-3360-2a6ae4d2e3702013-07-10T11:17:47-06:00<p>Yea I try to keep that in mind. I'm always slowed down when something is only in mm because I have to convert things by punching them into Google.</p>
Sleepwalker3 on PRT-10474 - XT60 Connectors - Male/Female PairSleepwalker3urn:uuid:ffd82aee-c198-1d69-48f1-2283806e5e572013-07-10T11:08:45-06:00<p>And very nice drawings they are too! You didn't forget us Metric people :)</p>
Sleepwalker3 on PRT-10474 - XT60 Connectors - Male/Female PairSleepwalker3urn:uuid:abca5f9e-9caf-c066-40df-196384954f5c2013-07-10T11:05:26-06:00<p>Thanks for the prompt response :) ...now you better go and have a beer too - Oh and buy Paul one for all his 2 years of slaving over a hot mouse!</p>
One Chris Two Chris Red Chris Blue Chris on PRT-10474 - XT60 Connectors - Male/Female PairOne Chris Two Chris Red Chris Blue Chrisurn:uuid:b4f0ae2e-78fe-7e92-fcd8-4b6f0c1d01cd2013-07-10T10:49:28-06:00<p>And they are up!</p>
RobertC. on PRT-10474 - XT60 Connectors - Male/Female PairRobertC.urn:uuid:2b27b6ec-16d8-3bcc-2993-6efcea8a15e62013-07-10T09:27:08-06:00<p>We use Photoshop for rulers.<p>As for the size, we never really did anything with it because they're very common and pretty standard in RC. But a drawing is actually coming soon.</p></p>
Paul Smith on PRT-10474 - XT60 Connectors - Male/Female PairPaul Smithurn:uuid:5830e6d0-78ab-91ef-a729-bf85348288742013-07-10T07:58:03-06:00<p>No worries! :)</p>
Sleepwalker3 on PRT-10474 - XT60 Connectors - Male/Female PairSleepwalker3urn:uuid:a4afda0c-b1a3-3bb5-f33a-4822b4e47fa22013-07-09T21:42:25-06:00<p>Your mouse must be worn out by now from all that CAD drawing ;), you'd better take a break and go have a beer. Actually I was just curious.</p>
Sleepwalker3 on PRT-10474 - XT60 Connectors - Male/Female PairSleepwalker3urn:uuid:45e05100-6361-8654-0da5-233701df83e72013-07-09T21:38:41-06:00<p>LOL, OK, it was only a joke! Sorry if I have a twisted sense of humour :) What would be useful for people though is just a photo with the usual ruler picture beside it, just so they can get a perspective of size. Unfortunately saying it's about the size of a dime is like me telling you it's the size of an Aussie 10c piece, but thanks for trying. By the way, what do you use to put those ruler dimensions in the pictures?</p>
Paul Smith on PRT-10474 - XT60 Connectors - Male/Female PairPaul Smithurn:uuid:713de202-2da2-93a1-4a0a-46d9abb9282a2013-07-09T14:34:29-06:00<p>I'm making them as we type! I've been at it for two years solid now, but check back tomorrow because they'll be done!</p>
RobertC. on PRT-10474 - XT60 Connectors - Male/Female PairRobertC.urn:uuid:400cd9e4-389a-5c3b-b52a-c80f226be41b2013-07-09T11:37:01-06:00<p>it hopefully will be. oddly enough, there are NO dimensional drawings available for these anywhere. we are still looking for SOME source, but even manufacturers claim they have no dimensions. I can tell you simply that they're about the size of a dime or so. They're just assumed as a 'standard' connector in RC applications, so everyone just takes the size for granted.</p>
dbvanhorn on PRT-10474 - XT60 Connectors - Male/Female Pairdbvanhornurn:uuid:93e8d79c-97a7-f9b6-32e9-ac717c0ca1ad2013-07-08T10:53:17-06:00<p>You could take a picture with it sitting on a US $0.25 piece. At least anyone worldwide can work it out from that.</p>
Sleepwalker3 on PRT-10474 - XT60 Connectors - Male/Female PairSleepwalker3urn:uuid:5d3992e7-6283-c802-8068-dd5b45b334e52013-07-08T10:15:41-06:00<p>...and still working on it - must be some drawing!</p>
Customer #255632 on PRT-10474 - XT60 Connectors - Male/Female PairCustomer #255632urn:uuid:c7d7a7f1-44ed-069f-173e-37a8bfb4a7c52013-06-15T15:13:39-06:00<p>To 65 Amps... and beyond!</p>
Funda on PRT-10474 - XT60 Connectors - Male/Female PairFundaurn:uuid:97a14360-60fe-bac8-cdf6-505e2f4af9c72013-05-22T11:00:28-06:00<p>We do not sell these separately, unfortunately.</p>
Customer #326474 on PRT-10474 - XT60 Connectors - Male/Female PairCustomer #326474urn:uuid:7e4ad8bf-a7c4-791b-155d-6432aca013a82012-08-03T07:56:15-06:00<p>For what it's worth, these can sort of fit 10 awg decently. Still not quite ideal for 65A, though. Depends in part how long you use the wire, what kind of casing the wire has, and what you're willing to tolerate in losses.<p>These xt60s are what I've been using for a long time; they're wonderful.</p></p>
Customer #326474 on PRT-10474 - XT60 Connectors - Male/Female PairCustomer #326474urn:uuid:bd1ad824-ac48-7f0a-9da8-8963f759db492012-08-03T07:51:54-06:00<p>Everyone has answered your question (and, well, it was a year ago)<p>But what you ask is precisely one of the benefits of these connectors. Neither side has exposed terminals.</p><p>However, with these batteries what looks like the female side is actually considered the male side, by hobbyking standards at least (a common place to buy LiPo batteries.) As such, the side that goes into the other side (which surrounds it) is the one that is considered the battery side piece. Erm, I dont know if I could have been worse at describing it.</p><p>But, one side fits into the other side. The side that fits into the other side is the battery side.</p></p>
Customer #312793 on PRT-10474 - XT60 Connectors - Male/Female PairCustomer #312793urn:uuid:1352879c-1692-177d-3388-fa3bb5c1c8232012-07-18T16:01:57-06:00<p>According to http://wiki.xtronics.com/index.php/Wire-Gauge_Ampacity you would need a 8 AWG wire to carry 65A. A 12 AWG wire max is 41A. Please be careful these are potentially dangerous current values.</p>
JohnGalt on PRT-10474 - XT60 Connectors - Male/Female PairJohnGalturn:uuid:3a34ee49-d28a-e7c1-0a70-3672c385dc5e2012-06-19T04:45:19-06:00<p>Can sparkfun offer these as singles, i.e. just a male by itself or just a female by itself (not in pairs)? I seem to always have one sex or the other of various connector types collecting somewhere after the mate goes off elsewhere.</p>
dbc on PRT-10474 - XT60 Connectors - Male/Female Pairdbcurn:uuid:f545423f-e7ff-8885-76f1-f8aa28dcb7f42011-08-27T13:45:29-06:00<p>Actually, my favorite connector for this kind of application is the Anderson PowerPole line of connectors, which can handle high currents quite easily. Good things about PowerPoles: 1) Easy to crimp, 2) hermaphrodite connector, so you don't have pairing issues, 3) shells in rainbow colors, 4) self-interlocking to make your own multi-conductor connectors. Not so good: 1) Crimping is only easy with the proper crimp tool, 2) not cheap, it costs a little more per contact than these XT60's.<br>
PowerPoles might make a good product for SparkFun to carry. There are crimp pins for various current ratings, many colors of shells, and pins for PCB mounting. The PCB pins and shells in colors other than red and black can be hard to come by in small quantities. Here is a little write up I did for the local robot club:<br>
http://hbrobotics.org/wiki/index.php?title=Anderson_PowerPoles</p>
ColinB on PRT-10474 - XT60 Connectors - Male/Female PairColinBurn:uuid:78fa1b35-b871-6bac-61a3-24e823b668482011-06-22T22:21:14-06:00<p>Certainly there must be a maximum current and maximum voltage rating for these. Does it really need to be “left as an exercise to the reader” to determine the maximum limits?</p>
stilldavid on PRT-10474 - XT60 Connectors - Male/Female Pairstilldavidurn:uuid:9563ea6b-4eb9-b289-8080-5c4e88a4a5192011-06-15T11:14:41-06:00<p>This way the battery won't short if it happens to bump into a piece of metal, which it could easily do (and start a fire!) if the male end was on the battery.</p>
RobertC. on PRT-10474 - XT60 Connectors - Male/Female PairRobertC.urn:uuid:663aec62-e3d0-aa02-fc0d-868a672dff002011-06-15T10:22:53-06:00<p>I see what you're asking. Traditionally, the female end goes to the battery.</p>
ctdahle on PRT-10474 - XT60 Connectors - Male/Female Pairctdahleurn:uuid:91c087ba-bd10-78a7-6a5e-7410f6b414e92011-06-15T09:52:49-06:00<p>Ooops, sorry, mis-read your question. Your assumption that "male contacts / female housing is for the load side" makes the most sense from a "don't put a battery pack in your pocket and short it on your car keys" viewpoint.</p>
RobertC. on PRT-10474 - XT60 Connectors - Male/Female PairRobertC.urn:uuid:f0a5c462-f930-4cd9-7b23-e513f9c13fef2011-06-15T09:48:59-06:00<p>We're working on making our own drawing for these.</p>
ctdahle on PRT-10474 - XT60 Connectors - Male/Female Pairctdahleurn:uuid:f114280f-2983-3cd6-83ae-9adf5f96bc802011-06-15T09:40:14-06:00<p>Look at the photo, + and - are molded on the housing.</p>
Quazar on PRT-10474 - XT60 Connectors - Male/Female PairQuazarurn:uuid:8e701e29-95a1-7841-2d9a-794ddd66cdb22011-06-13T13:08:40-06:00<p>What is the standard polarization and "direction" for these when using them with a battery pack? I'm assuming the male contacts / female housing is for the load side, and the female contacts/ male housing are for the battery side.<br>
It would be nice for the defacto standard to be mentioned on the product page to simplify this decision for everybody.<br>
Cheers,<br>
- Dean</p>
Reed on PRT-10474 - XT60 Connectors - Male/Female PairReedurn:uuid:c0c3a81f-897b-0049-f291-8b177d7c41542011-06-12T04:40:42-06:00<p>Agreeing on need for pictures with rulers involved, for now I'll just assume they're smaller than a toaster and larger than a grain of rice.</p>
xieliwei on PRT-10474 - XT60 Connectors - Male/Female Pairxieliweiurn:uuid:da8641dc-10ca-884c-d542-f5d34336e01b2011-06-11T11:10:21-06:00<p>Erm, up to and beyond 65A continuous draw? Does that mean it can do 1000A? =)</p>
Shavi on PRT-10474 - XT60 Connectors - Male/Female PairShaviurn:uuid:da01b870-eb0e-36ae-4da5-0ef35a486cf02011-06-10T23:17:15-06:00<p>Datasheet is hard to come by, from what I could find:<br>
Dimensions :<br>
Female side : L 20mm x W 15mm x H 8mm<br>
Male side : L 20mm x W 15mm x H 8mm<br>
Total Length when conneted together : L 33mm<br>
original manufacturer: Amass</p>
TeslaFan on PRT-10474 - XT60 Connectors - Male/Female PairTeslaFanurn:uuid:0288ebdf-a44a-9c4a-a5bb-88ce3c2fe0172011-06-10T15:45:40-06:00<p>i like that you're starting to put out male / female inline connector sets, something of a hole in your product line. Now I don't have to order as many parts from Mouser.</p>
RobertC. on PRT-10474 - XT60 Connectors - Male/Female PairRobertC.urn:uuid:1b81ea10-2703-501b-32e0-d272158aef802011-06-10T12:17:43-06:00<p>XT60 connectors are standard sized. Let me see if I can track down a generic datasheet.</p>
Marcoose on PRT-10474 - XT60 Connectors - Male/Female PairMarcooseurn:uuid:e1a367cd-dff9-a4d7-8815-808aa4cf06ff2011-06-10T12:13:43-06:00<p>At least photo with the rulers to give idea of physical size :)</p>
frank26080115 on PRT-10474 - XT60 Connectors - Male/Female Pairfrank26080115urn:uuid:9fa8666e-8039-47c0-96f1-5a15f9092f0b2011-06-10T11:22:04-06:00<p>You will not be able to crimp these.<br>
Make sure you use heat shrink tubing, electrical tape is not a good idea with these.</p>
Jay2 on PRT-10474 - XT60 Connectors - Male/Female PairJay2urn:uuid:10cdbb59-60ef-8e74-1d9a-ca42557554902011-06-10T10:53:49-06:00<p>Datasheet PLEASE!</p>
russd13 on PRT-10474 - XT60 Connectors - Male/Female Pairrussd13urn:uuid:6af0dd2c-2e1f-f838-8f2e-189eab60818b2011-06-10T10:27:35-06:00<p>They can take a 12 gauge wire. You solder the wire to these connectors.</p>
MattQ on PRT-10474 - XT60 Connectors - Male/Female PairMattQurn:uuid:93ea9452-5682-5ba8-eac0-0e668694c11e2011-06-10T09:15:59-06:00<p>what gauge wire do these connectors take? Do they need to be crimped, or are they designed to be soldered to directly?</p>