SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T10:49:22-06:00SparkFun ElectronicsCustomer #336162 on COM-10509 - Relay SPDT Sealed - OmronCustomer #336162urn:uuid:088a219e-9341-d153-fcb6-a46fb8bb3d112013-04-04T17:40:22-06:00<p>…</p>
chucho on COM-10509 - Relay SPDT Sealed - Omronchuchourn:uuid:d939bd66-b278-c673-e525-e80010f8e9872012-04-15T21:28:00-06:00<p>I am working on an arduino motion detector. Everything works. I want to change so that a speaker connected to a separate 9V battery sounds when Arduino senses movement from PIR. I need relay that is triggered from the 5v arduino after a digital high is sensed.<p>Can you guys help me know if this would work?</p></p>
Bravo Sierra on COM-10509 - Relay SPDT Sealed - OmronBravo Sierraurn:uuid:0fb747a3-56a6-68c2-31b6-7f2fcc4047002011-12-05T04:41:08-07:00<p>This relay is rated for 5A. So 600W on a 4Ohm element is:
I=√(600/4)=12,24A
U=√(600*4)=48,98V<p>So this relay is to small, I think <a href="http://www.sparkfun.com/products/10924" rel="nofollow">this relay</a> is better fit for the job.</p></p>
LeighLee on COM-10509 - Relay SPDT Sealed - OmronLeighLeeurn:uuid:703e24a6-3bfe-0b4f-7542-d311abc2de0c2011-11-17T10:21:05-07:00<p>I am looking for a relay that can handle 600W amplifier for two 4 ohm speakers.
Can this product handle it or do you have a product that does it?
Thank you!</p>
ethan.ferrell on COM-10509 - Relay SPDT Sealed - Omronethan.ferrellurn:uuid:2cf5cdab-e7a8-83b9-ccde-d4f6c50c5bdc2011-08-15T09:08:28-06:00<p>Omron doesn't make a 3.3v version according to the datasheet.</p>
roycohen2013 on COM-10509 - Relay SPDT Sealed - Omronroycohen2013urn:uuid:075b598f-3a6b-a092-94a6-4cdbc96cc7c72011-02-16T15:03:29-07:00<p>are you guys also gona bring a 3.3 version of this or somthing similar because i always have trouble finding them in places that arent digikey</p>