SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T09:29:22-06:00SparkFun Electronicsgumush on PRT-10592 - Coin Cell Battery Holder - 12mm (SMD)gumushurn:uuid:c4dd87ea-0ccf-0ab0-0282-b2948fd125482013-02-14T04:30:11-07:00<p>Upps , i found it, thanks.</p>
Kamiquasi on PRT-10592 - Coin Cell Battery Holder - 12mm (SMD)Kamiquasiurn:uuid:dd7125e3-80e1-dccf-55ca-35bcab4382042013-02-14T04:21:10-07:00<p>You'll have to double-check, but it should be:<br>
SparkFun-Electromechanical.lbr<br>
Device: BATTERY<br>
Package: BATTERY12MM</p>
gumush on PRT-10592 - Coin Cell Battery Holder - 12mm (SMD)gumushurn:uuid:d3875107-ab77-a0a3-52c0-5f10395633722013-02-14T03:27:25-07:00<p>Is these part have a datasheet. O couln't find these part in sparkfun library ?</p>
Segphalt on PRT-10592 - Coin Cell Battery Holder - 12mm (SMD)Segphalturn:uuid:93842bd9-0125-109c-c7c5-f79b5d0660df2011-10-24T03:41:41-06:00<p>I ordered some likes these from digikey and one note for potential buyers. They tend to lift pads, since the battery is being held in by the tension between the board and the contacts on the holder. Even using a through hole point with solder all the way through it will still lift pads on even fab house boards. I have had 2 boards that have never had a single pad lifted by them, and about 10 boards that after a while the pads just pop making them unusable.<br>
They don't stay even remotely if you only have solder on one side without the through hole added support.<br>
My advice, use the through hole parts, they stay in place and if you needed one side nice and flat like I did you can trim the short before soldering and maintain a fairly planar surface on the opposing side.</p>
BB on PRT-10592 - Coin Cell Battery Holder - 12mm (SMD)BBurn:uuid:378896ab-eb77-cce3-ad19-55188d0e18452011-04-01T11:02:07-06:00<p>Awesome, it looks like a cartoon cat!</p>
JCWoltz on PRT-10592 - Coin Cell Battery Holder - 12mm (SMD)JCWoltzurn:uuid:00e93df7-bed9-8f12-f812-8e6dd32d28232011-03-31T21:17:52-06:00<p>Will the SFE Eagle library be updated to include this and the other new parts you have added since April 13th 2010? please?</p>