SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-19T00:13:39-06:00SparkFun ElectronicsAsh.j on TOL-10721 - Soldering Tip - Hakko - Conical (T18-B)Ash.jurn:uuid:8799a363-6b1b-2e47-ccaf-6b6fd3edc4c22013-12-10T21:14:33-07:00<p>what is the difference between hakko and plug type tips?</p>
Uze on TOL-10721 - Soldering Tip - Hakko - Conical (T18-B)Uzeurn:uuid:db212744-ff9f-cf75-a6a7-5e66e7c969492012-09-05T19:13:14-06:00<p>This tip <em>is not</em> the one that shipped with my FX-888. Instead it was the Chisel (T18-D16).</p>
skazahay on TOL-10721 - Soldering Tip - Hakko - Conical (T18-B)skazahayurn:uuid:9be3b59f-3ce8-afda-a312-53721e03d4a02012-03-16T00:01:47-06:00<p>This fit perfectly on my 907 Iron, used with a Hakko 936.
It appears to be the same in/out diameter compared to the tip that came with the iron originally (T18-D16).</p>
danvm on TOL-10721 - Soldering Tip - Hakko - Conical (T18-B)danvmurn:uuid:d8e6e493-a5d9-ca2e-32da-d39c2c8eb5b62012-01-17T08:19:07-07:00<p>No, the inner diameter is smaller on 888 tips. The heating element won't fit in it.</p>
Blueblast88 on TOL-10721 - Soldering Tip - Hakko - Conical (T18-B)Blueblast88urn:uuid:55d0e178-3b34-2b2c-bcd4-3752386c54e72011-10-10T20:37:18-06:00<p>will this work with the hakko 936b?</p>
Bpaton on TOL-10721 - Soldering Tip - Hakko - Conical (T18-B)Bpatonurn:uuid:aa53083f-f5c9-972b-8584-a2fb203286502011-06-09T23:00:37-06:00<p>The Dimensional Drawing link is not quite right I get this when I click on it:<br>
This XML file does not appear to have any style information associated with it. The document tree is shown below.<br>
−<br>
AccessDenied<br>
Access Denied<br>
9CC43FA3B9B6F106<br>
−<br>
HyQwzo0C/uRHOyqxVmMKJ3HaHhGO8mGEgl/m/MfBbnF987u2Ec2yqeqkrhP9caCt</p>