SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T01:18:04-06:00SparkFun ElectronicsDoctor Who on RTL-10776 - RedBoard - PTH Kit RetailDoctor Whourn:uuid:36bf828c-8cd8-4fd9-6e14-9c3a389f53602019-06-11T23:16:39-06:00<p>What we need is to have either this fellow, or its regular one reintroduced in the stream for the currently new retail vendor.</p>
WemblyTinkerer on RTL-10776 - RedBoard - PTH Kit RetailWemblyTinkererurn:uuid:2f0246dc-9190-4565-975d-d2f0b0ee86092012-12-05T16:12:46-07:00<p>This is a nice kit. the instructions are good. the board is solid. It works as advertised. However, I made a boo boo. I went and put a wrong cap around the crystal. so it stops oscillating after a bit. It works fine until the clock stops though. I'm going to fix the error when the parts I ordered come in. The numbers on the disc capacitors are insanely tiny. May I suggest that you mark or bag the 22pf caps so they are easier to sort from the .1mf ones. thanks much for great fun stuff,
tap</p>