SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T20:12:43-06:00SparkFun ElectronicsCustomer #382085 on ROB-10826 - Robotic Claw Pan/Tilt BracketCustomer #382085urn:uuid:90cec910-c06a-d7a0-f27a-cc3065dc3b502012-12-07T10:25:23-07:00<p>what is used on back side of tilt servo</p>
Customer #356786 on ROB-10826 - Robotic Claw Pan/Tilt BracketCustomer #356786urn:uuid:c0db1b6a-b381-e5f6-1602-81813935f8152012-09-13T14:43:00-06:00<p>Does anyone know which enclosure is used in the last photo? Thanks!</p>
Sofia on ROB-10826 - Robotic Claw Pan/Tilt BracketSofiaurn:uuid:53321dd9-85ce-888b-fb8a-68d2f609fcda2012-06-16T13:03:52-06:00<p>Can we get the arduino sketch, schematic, & other info on how to make the claw setup that you have in the last pic.</p>
Sofia on ROB-10826 - Robotic Claw Pan/Tilt BracketSofiaurn:uuid:78d3db70-987e-cd85-0a02-44bb5cc5626a2012-06-16T13:02:11-06:00<p>Now all we need is an arduino sketch for that layout & a schematic on how to put everything together, 'cause I'd really love to have that on my work bemch.</p>
JakeR on ROB-10826 - Robotic Claw Pan/Tilt BracketJakeRurn:uuid:c3104bc1-1d91-b19b-e32f-d13a23afdef92012-05-09T17:14:08-06:00<p>A team of students and I built a robotic arm using this plus the claw. It was a great product for us especially given our budget. Check it out <a href="http://www.youtube.com/watch?v=ouTSRdDt448&feature=colike" rel="nofollow">here</a>.(youtube)<p>One tip: We had issues where when the claw was mounted the large tilt servo would become almost uncontrollable. Physical resonance in the system matched up with that of the servo. The servo would see a spike in the claw's motion and kick back the other way to stop it. Instead of this damping out to nothing as usual the condition would perpetuate itself. To fix it we just removed the 4 screws that attach the servo to the outside U bracket. With these removed the issue stopped and the arm was still quite secure.</p></p>
rwaldron on ROB-10826 - Robotic Claw Pan/Tilt Bracketrwaldronurn:uuid:75b4aa72-03ed-3d26-3674-b7a5417d40d12012-04-10T15:08:59-06:00<p>Does anyone have a link to the bottom/base that is shown in the last photo?</p>
Customer #258107 on ROB-10826 - Robotic Claw Pan/Tilt BracketCustomer #258107urn:uuid:5a6ef213-de93-0c70-2a4a-9e4c0914ecf82011-11-28T17:50:06-07:00<p>Hello, I was wondering if this came with two servos, the pan one and the tilt one. It seems like it should given the $30 price. Also, is another servo required to operate the claw? So three servos in total, am I correct?
Thanks for your help.</p>
Customer #258107 on ROB-10826 - Robotic Claw Pan/Tilt BracketCustomer #258107urn:uuid:935e463f-2de7-3fa2-eb8a-1f499d1b847c2011-11-28T17:50:06-07:00<p>Hello, I was wondering if this came with two servos, the pan one and the tilt one. It seems like it should given the $30 price. Also, is another servo required to operate the claw? So three servos in total, am I correct?
Thanks for your help.</p>
RobertC. on ROB-10826 - Robotic Claw Pan/Tilt BracketRobertC.urn:uuid:38b0f7e3-aba0-953c-25cd-b3d175c631b92011-10-11T16:16:31-06:00<p>0.3075 lbs.</p>
N314 on ROB-10826 - Robotic Claw Pan/Tilt BracketN314urn:uuid:9c8856e6-24bb-1bbf-775e-4a59944fd1602011-10-11T15:30:53-06:00<p>Any idea how much this weighs?</p>
David C Dean on ROB-10826 - Robotic Claw Pan/Tilt BracketDavid C Deanurn:uuid:3aad681a-d225-42bd-9706-af1717f0f55c2011-09-19T14:46:54-06:00<p>I don't know. I think the claw is $10. So $30 for two job specific brackets, a servo, all mounting hardware and wrench doesn't seem too bad. It looks like the servos alone go for $11 on SFE.</p>
stewie0056 on ROB-10826 - Robotic Claw Pan/Tilt Bracketstewie0056urn:uuid:d82d5b17-a186-5a69-73e1-bbeabe63a6082011-09-19T10:11:59-06:00<p>the title is misleading. when i first read this i assumed the robot claw is included.</p>
SomeGuy123 on ROB-10826 - Robotic Claw Pan/Tilt BracketSomeGuy123urn:uuid:0de5a607-ca44-a0b3-8436-bd05dbe4b4632011-09-17T19:56:39-06:00<p><a href="http://www.sparkfun.com/news/707#comment_46487" rel="nofollow">These comments</a> on the new product post provide some additional information about the product.</p>
Customer #203771 on ROB-10826 - Robotic Claw Pan/Tilt BracketCustomer #203771urn:uuid:a25661f8-7af5-785e-2280-719d05ceeea12011-09-17T01:05:24-06:00<p>its funny i would pay at least 30 for the claw, and maaaaaaaaaybe 10 for this pan tilt thing.</p>
RobertC. on ROB-10826 - Robotic Claw Pan/Tilt BracketRobertC.urn:uuid:c9898282-2095-caca-e54a-27303d6f9b0e2011-09-16T15:49:11-06:00<p>Everything but the last picture of the fully built arm. It includes the main body bracket with servo, the other rotating bracket, and all the hardware shown in the 4th picture.<br>
I'll get a picture of just this bracket built up so you can see what it looks like alone when it's assembled.</p>
Davemaster on ROB-10826 - Robotic Claw Pan/Tilt BracketDavemasterurn:uuid:5ee4c33b-297c-7bf6-f687-ad3d096f5c3e2011-09-16T14:08:44-06:00<p>Greetings,<br>
What exactly this item includes: how many parts/servos...<br>
Thanks a lot</p>
RobertC. on ROB-10826 - Robotic Claw Pan/Tilt BracketRobertC.urn:uuid:c500e11a-c5c5-016a-c7e7-7011df98a69d2011-09-15T18:07:56-06:00<p>It's just a PCB used as a base for the pan servo.</p>
SomeGuy123 on ROB-10826 - Robotic Claw Pan/Tilt BracketSomeGuy123urn:uuid:c31601dc-1549-fc18-24b0-da76ed52ac812011-09-15T18:04:06-06:00<p>What is that board at the base of the arm assembly?</p>