SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T05:28:37-06:00SparkFun Electronicsrcox on COM-11146 - Toggle Switch Cover - Waterproofrcoxurn:uuid:4e598c3f-a59f-e597-3f10-40d42021794d2014-07-24T11:58:51-06:00<p>I don't normally do this, but since I needed this part and there was no prediction for when it would be in stock, I found it on Parts Express: https://wholesale.parts-express.com/switch-boot-with-retention-washer--060-589 It's a little more expensive there and you have to pay their shipping. Since I can normally pick up directly from SparkFun I would continue buying these from them if they return to stock.</p>
Customer #549878 on COM-11146 - Toggle Switch Cover - WaterproofCustomer #549878urn:uuid:62b1a904-8c8c-0b47-45ad-7743ffff39bd2014-04-30T15:28:00-06:00<p>is this dust proof?</p>
DrewMangus on COM-11146 - Toggle Switch Cover - WaterproofDrewMangusurn:uuid:ca03b2ba-f21f-daae-8cd5-8bc116db2be02013-07-30T14:12:01-06:00<p>There is a Metal Nut underneath.</p>
DrewMangus on COM-11146 - Toggle Switch Cover - WaterproofDrewMangusurn:uuid:4d6e5773-6f56-6786-dbd5-411e063d70642013-07-30T14:11:14-06:00<p>Yes, they will indeed.</p>
Customer #312338 on COM-11146 - Toggle Switch Cover - WaterproofCustomer #312338urn:uuid:a8320014-9cd0-2eab-ad83-2613eeba6f6b2013-03-26T07:50:43-06:00<p>Is this all rubber or is there a metal nut underneath? A photo of the underside would be helpful. What is the construction material?</p>
Customer #418000 on COM-11146 - Toggle Switch Cover - WaterproofCustomer #418000urn:uuid:73294aef-2e57-78b6-a6c3-4a9d75fedc9e2013-03-11T19:14:20-06:00<p>Will one of these fit under a missile switch cover?</p>
kjmccarx on COM-11146 - Toggle Switch Cover - Waterproofkjmccarxurn:uuid:97973297-fc6b-5d8a-57f6-8537e6fadd8c2012-08-15T13:26:45-06:00<p>Lol. Not only does it look like a condom. But they also made a condom reference in the description. Gotta love sparkfun.</p>