SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T09:05:12-06:00SparkFun ElectronicsCanCerManNor on SEN-11171 - FlyCamOne eco V2CanCerManNorurn:uuid:f9c7bc39-edb6-5bbf-0768-74bb929c655a2014-09-28T10:53:34-06:00<p>Is is possible to split a bigger card up in multiple sections and do somekind of script so it continue to record after a section is full until all sections are full? is there a possibility to add wifi,bluetooth? Can it be used with any kind of sensor like lightsensor etc?</p>
qqrs on SEN-11171 - FlyCamOne eco V2qqrsurn:uuid:84c80000-a03c-4a4c-0d95-cf2dbb4820892014-08-12T11:22:39-06:00<p>The first unit I received had a color problem (moiré pattern effect) which was resolved with a quick replacement from SparkFun (thanks!).<p>Firmware upgrade on Windows 7 was a bit tricky but I ended up getting it to work with Fiskbil's suggestion below to press F8 on boot and select “Disable Driver Signature Enforcement”. Also, it seems USB power was not sufficient to upgrade firmware since it didn't work until I plugged in a charged battery (though that could have been a fluke).</p><p>I haven't used the camera much yet but my first impression is that image and video quality aren't amazing but are better than nothing and acceptable for my use given the low cost and small size. Think older webcam, not GoPro.</p><p>The camera supports charging the connected battery when power is available via USB.</p></p>
Fiskbil on SEN-11171 - FlyCamOne eco V2Fiskbilurn:uuid:08d2c84e-7a54-1255-edba-b7250e0c2ec62014-05-25T10:47:04-06:00<p>On Windows 7 and newer you need to disable the driver signature check. Do this by rebooting Windows, press F8 after the bios screen and select "Disable Driver Signature Enforcement". Windows now boots up as normal and the driver should work.</p>
Customer #452955 on SEN-11171 - FlyCamOne eco V2Customer #452955urn:uuid:de2d11d7-b408-c647-cc12-ef17216218c72014-04-10T14:49:15-06:00<p>Hello Baz0unga,<p>I am FlycamoneV2 in my project, i am using PIC18F458, I don't know how to control the PWM signal through the PIC and also the wire connections(How do i connect the Flycam to PIC). Can anyone Please help me out.</p></p>
Customer #452955 on SEN-11171 - FlyCamOne eco V2Customer #452955urn:uuid:0c40b688-ac2f-302a-406b-64b4dbe451782014-04-10T14:47:40-06:00<p>Hello Everyone,<p>I am FlycamoneV2 in my project, i am using PIC18F458, I don't know how to control the PWM signal through the PIC and also the wire connections(How do i connect the Flycam to PIC). Can anyone Please help me out.</p></p>
Jeraz on SEN-11171 - FlyCamOne eco V2Jerazurn:uuid:21a88467-ccec-4488-2572-1a511c28d8de2014-02-20T16:46:02-07:00<p>Do we have to set the modes every time on a fresh start or does it remember the previous set mode??
Whats the delay between switching it on and the instant it starts recording or any other set mode?<p>Thanks!</p></p>
Jeraz on SEN-11171 - FlyCamOne eco V2Jerazurn:uuid:d0db1dde-e4d4-225b-dee4-ce7886f31c4e2014-02-20T16:45:00-07:00<p>Two Questions:
Do we have to set the modes every time on a fresh start or does it remember the previous set mode??
Whats the delay between switching it on and the instant it starts recording or any other set mode?</p>
arobose on SEN-11171 - FlyCamOne eco V2aroboseurn:uuid:90900c5c-8e81-924e-81f3-0bb680ce7b252014-02-03T05:38:16-07:00<p>Could you please tell me what is the reference of the LIPO battery connector of the board as it's not an usual JST connector for LiPo battery (PRT-09749) proposed for example in the Lithium Polymer USB Charger and Battery (RTL-09876).
Thanks for answer</p>
Customer #484278 on SEN-11171 - FlyCamOne eco V2Customer #484278urn:uuid:29a14681-37c2-e9d1-1eca-caf41f07e2822014-01-16T15:26:40-07:00<p>Just got one today and the on off switch does not work and when connected to the power source it goes on just sometimes. DONT BUY IT. I am posting a video on youtube showing the problem - flycamonev2_becker</p>
Purple People Eater on SEN-11171 - FlyCamOne eco V2Purple People Eaterurn:uuid:76b8c7bc-8011-9738-b225-9a4e665fbbf22013-11-21T12:43:29-07:00<p>Can you do that?</p>
Spokkam on SEN-11171 - FlyCamOne eco V2Spokkamurn:uuid:e09ba9d9-97ad-7237-e09f-cbb65b2360ab2013-07-22T16:29:05-06:00<p>Had some problems with this. It was working perfectly up until I installed the drivers. When I went to reboot I switched the on/off and held down the button as was said. When that chose to fail I unplugged it and tried some more times unsuccessfully. Eventually I gave up and resigned myself to the original settings.
The footage is decent and acceptable with the original settings unless you're willing to spend over four times the price on the similar HackHD camera which is also available.</p>
Spokkam on SEN-11171 - FlyCamOne eco V2Spokkamurn:uuid:f979522a-b3c4-6b20-c0f0-1402c1dc18da2013-07-22T15:19:50-06:00<p>Don't worry, solved it. :)</p>
Spokkam on SEN-11171 - FlyCamOne eco V2Spokkamurn:uuid:fe3e8c98-ecb9-880f-b061-d4543e165bc62013-07-22T12:15:03-06:00<p>Is it possible to connect this to a breadboard and supply the right current through regular li-ion batteries instead of having a li-poly battery?</p>
Customer #451657 on SEN-11171 - FlyCamOne eco V2Customer #451657urn:uuid:fb2bbd1f-713f-11db-ae7d-f99178f4cabe2013-07-03T15:10:57-06:00<p>I've had no luck, spent hours; followed the instructions to the letter. Nothing, just odd messages and a virus warning!<p>Is there a better way? are there instructions that work?</p><p>Just started everything from scratch - only errors. This feature is a waste of time.</p></p>
Customer #17759 on SEN-11171 - FlyCamOne eco V2Customer #17759urn:uuid:f1ec7d5a-0265-8ba6-d7cf-e9a7a290ba252013-06-23T03:07:08-06:00<p>Hello, I have a dell win 7 machine and cannot get the update to higher resolution on the FlyCamOne V2 to work. The first half of loading the driver works ok. After rebooting, I held the white button down and plugged in the USB cable. Got error message about driver working correctly. Starting the second driver install program and got "Device can't be initialized. Please check driver or hardware settings." What should I do next? Thanks.</p>
Oxameter on SEN-11171 - FlyCamOne eco V2Oxameterurn:uuid:a2a7842e-cb38-f625-e24e-ce375f9d233a2013-06-11T12:06:46-06:00<p>Just fyi it appears to use about 150mA</p>
SixEcho on SEN-11171 - FlyCamOne eco V2SixEchourn:uuid:c1a70e01-5edb-68b5-4211-56aeed14c3c32013-03-06T00:08:35-07:00<p>I bought one of these and I cannot get it to turn on. Tried using a model helicopter li-po single cell, and also regulated dc. An LED turns on when I connect it to the computer, but that's it. Did anybody else have this problem? Does anyone know if it can be fixed?<p>thanks!</p></p>
Baz0unga on SEN-11171 - FlyCamOne eco V2Baz0ungaurn:uuid:4881f4bc-0aaa-a19d-2e8c-6b84707ffc622013-03-05T03:27:47-07:00<p>No i haven't tried. I do not know if NTFS is supported by this camera, i will have a look.
But you are right, FAT32 specifies a maximum file size of (4GB) 2^32 bytes.
The firmware does not automatize recording continuation after the first 4GB of recording, creating a new file. Most people do not need that, but i do !</p>
Customer #393864 on SEN-11171 - FlyCamOne eco V2Customer #393864urn:uuid:d54b16c4-fade-0988-bb36-cc51a0469fab2013-02-10T17:04:08-07:00<p>Is there any way to stream the feed to an X-bee or an Arduino? On my mobile rover platform, It would be great to be able to stream photos or videos without having to collect the SD card each time I wanted to review the pictures.</p>
AeroGuy_123 on SEN-11171 - FlyCamOne eco V2AeroGuy_123urn:uuid:9788f12d-c352-bb12-cd70-ac8de94329af2013-02-08T11:40:40-07:00<p>Thank you! That explains why.
Regarding your 4GB problem, I'm guessing it has to do with your SD card. Did you try formatting it to NTSF?</p>
Baz0unga on SEN-11171 - FlyCamOne eco V2Baz0ungaurn:uuid:5bbdec2a-d664-a4b7-8797-cf24d56584f32013-02-08T03:07:22-07:00<p>This is not possible with this camera. USB port just allow to handle your camera as a USB stick in order to download recordings.
Several other products are much more suitable for what you want to do.</p>
muRata on SEN-11171 - FlyCamOne eco V2muRataurn:uuid:8170ca1e-3998-3930-039c-8c27738c9ad12013-02-06T17:20:23-07:00<p>I looked at the website of the company that makes these, Is there a way that Sparkfun could get the 1080p version of these?</p>
Baz0unga on SEN-11171 - FlyCamOne eco V2Baz0ungaurn:uuid:2e7f2f43-8e2d-28a9-ec04-f2b999eed5b82013-02-03T10:36:04-07:00<p>AeroGuy,<p>I have done such thing with a PIC micro-controller two years ago, it is very stable. The problem that still remains is that even if they say that 8 GB cards are supported, the video recording stops after 4GB. Could'nt figure it out why, i suspect the firmware to be buggy.</p><p>However and like you, I experienced come trouble to make it properly work. I finally figured out that it is not enough to mimic PWM signal to get on/off/changeMode. You have also to generate the idle signal for a little time (half a second) before sending the trigger signal. If not the flycam will not obey.</p><p>I just made this code compliant with Arduino (to drive several cameras embedded in a weather balloon).
If you are interested in, just have a look at my Github repo.
https://github.com/sebastienjean/arduino-yasolibs</p></p>
Customer #404145 on SEN-11171 - FlyCamOne eco V2Customer #404145urn:uuid:04a33cda-53e8-515d-1115-27d10ec5fb6d2013-01-31T05:24:40-07:00<p>Hi<p>I would like to know if there is a way to read the vidéo in real time with the USB mini, so we can send it via radio. The aim is being able to see what a drone see, to aim properly the camera.</p><p>Thank you for the answer</p></p>
AeroGuy_123 on SEN-11171 - FlyCamOne eco V2AeroGuy_123urn:uuid:118c5962-4aaa-776d-c5a3-354c006556182013-01-11T13:17:45-07:00<p>Hello guys,<p>I am having a bit of trouble controlling this camera correctly. Have done a lot of testing with it and still cannot figure out what exact PWM it expects to turn the camera on/off. I would like to use it with an arduino and not an RC controller.</p><p>By the way, I also tried replicating an RC controller PWM with an arduino, this way it turns on/off unexpectedly. So any helpful tips are greatly appreciated.</p><p>Thanks!</p></p>
TechChimp on SEN-11171 - FlyCamOne eco V2TechChimpurn:uuid:792fe3e7-9583-9770-052d-747c5acb6d572012-12-15T14:46:04-07:00<p>Depends...might be D-1, which is 720x480 stretched for NTSC and is not 480P. Even in the days before DTV signals, it was impossible to get people to get the various screen resolutions correct. I applaud you for trying...</p>
pion on SEN-11171 - FlyCamOne eco V2pionurn:uuid:f3fe510e-c304-12d2-a043-d170716fb4822012-12-07T13:33:26-07:00<p>Does anyone know about the low-light performance of this? Is there an infrared filter in place, or would this camera pick up nighttime video with enough infrared light?</p>
ddegn on SEN-11171 - FlyCamOne eco V2ddegnurn:uuid:dc012410-f4b1-5fcf-3d71-fb72d0ae6dbc2012-10-08T21:12:11-06:00<p>The SD card socket has exposed solder connections after removing the white "wrapper". You could also tap into the SD card signal by using a uSD card sniffer. Tapping into the SPI signal is unlikely to do much good since the photo (or video) will be compressed and would require a much more powerful processor than an Arudino to make sense of the data.<p>I doubt there is Arduino code for decoding a JPEG file.</p><p>You'd also have a problem of where to hold an image inside the Arduino. The Uno has 32K of RAM and a still image is 72K in size.</p><p>SparkFun does sell a LinkSprite camera that sends a JPG photo over a UART. You'd still have the problem of storing a decoding a JPG but communication with the camera would be easier than communicating with this camera.</p></p>
jago lee on SEN-11171 - FlyCamOne eco V2jago leeurn:uuid:32e57150-40a1-e0cf-1b6e-89601a5801f12012-09-11T01:22:24-06:00<p>I really needed one of these a week ago, somone stole my waterman hemisphere. :(</p>
Customer #197750 on SEN-11171 - FlyCamOne eco V2Customer #197750urn:uuid:bde17e6b-f943-80dc-744a-9cc50018a5a62012-09-10T19:57:01-06:00<p>Hey all, I picked up one of these and love it, here's a video I shot with it on my quadcopter:
http://www.youtube.com/watch?v=boOw4qGnCQY
Hope it gives you an idea of how well it works, especially because the example footage is 404-ing.</p>
RobertC. on SEN-11171 - FlyCamOne eco V2RobertC.urn:uuid:b3ec179d-7016-b49d-ecd2-da3e8b00e0932012-07-30T09:24:27-06:00<p>It's the same resolution I believe. It's limited by the sensor.<p>As for the SPI question, I really don't know. Looks like you might have to get one and tinker around with it :-)</p></p>
baum on SEN-11171 - FlyCamOne eco V2baumurn:uuid:b4760f1b-5117-24a9-7c9e-49c496ff97ef2012-07-29T20:09:36-06:00<p>Pearce was able to get 20 min/2GB, so you can get 10min per gigabyte. 80 minutes for 8 GB.</p>
baum on SEN-11171 - FlyCamOne eco V2baumurn:uuid:587c893b-b283-ef29-c10d-d12935db022e2012-07-29T20:08:19-06:00<p>How fast? 30 fps may be impossible, but an image or two/second might be doable... but not easy.</p>
STARscream on SEN-11171 - FlyCamOne eco V2STARscreamurn:uuid:2d4ac1e7-acfb-9d9e-38d5-88856365a1242012-07-29T00:16:48-06:00<p>What is the resolution of this camera when you click a photo? is it remains the same as 720 x 480px or it will increase?<p>also i want to hack the sd card to be read by the arduino ,so as you have seen this module ,what you think? Will i be able to access the SPI bus of the SD card?</p></p>
PhilWheat on SEN-11171 - FlyCamOne eco V2PhilWheaturn:uuid:6c8d05d8-76af-7c8b-be1c-000b916bb3bc2012-07-04T14:07:39-06:00<p>I've had trouble as well. I'm just coming back to the site to try again, but so far haven't been thrilled with the unit.</p>
Customer #333006 on SEN-11171 - FlyCamOne eco V2Customer #333006urn:uuid:a61095f2-f9e0-199a-649b-39f88d78d48b2012-06-21T17:04:47-06:00<p>Can it communicate with a uC instead of using SD???</p>
SebCestBien on SEN-11171 - FlyCamOne eco V2SebCestBienurn:uuid:3b128c52-435d-bfdd-617a-1263fa3f3aad2012-06-12T00:43:25-06:00<p>Is the image in the SD card is accessible by an arduino? (by SPI for exemple)
or can I read still image from an arduino ?<p>I want to use this cam for processing an image image AND record video on SD card...</p></p>
Customer #330027 on SEN-11171 - FlyCamOne eco V2Customer #330027urn:uuid:576eaa36-6aae-ce51-e3ff-48107efc18e22012-06-09T18:16:22-06:00<p>there is how to make the camera images to be received on computer to remotely?</p>
pingy on SEN-11171 - FlyCamOne eco V2pingyurn:uuid:8161db73-a8ea-d8b0-3a32-fd3cea37eb2d2012-06-08T21:34:26-06:00<p>Has ANYONE actually gotten the firmware to update on their FlyCamOne?<p>I thought the hardest part would be tracking down a windows machine. Boy was I wrong!</p><p>I have a windows XP laptop; nothing special, and have not been able to get the firmware to update for the life of me. Been at it on/off for like 2 hours. It really should not be this hard.</p><p>The first couple of tries...I'll admit I didn't inspect the names of the files THAT carefully. The two files you are to use are VERY similar in naming convention.</p><p>Once I noticed the naming mix up I tried again 3x and still have no idea if it even worked. I was not prompted in the way the readme.txt tells me I should be, so I assume the firmware did not take.</p><p>wow what a difficult process. I was hoping to take my FlyCam on my madien air plane flight. rigged it up to be strapped to my head. I suppose Im either going to have to postpone my flight or go with lesser res. :*(</p></p>
ATtiny Fan on SEN-11171 - FlyCamOne eco V2ATtiny Fanurn:uuid:2b52c152-0533-51ff-4d3f-cdc7435bb4b22012-05-31T08:07:45-06:00<p>No, full color.</p>
DaGlitch on SEN-11171 - FlyCamOne eco V2DaGlitchurn:uuid:6a35bc75-4cb5-a8e7-1211-b11d43f5b5982012-05-23T21:43:03-06:00<p>^- This :)</p>
Pyrofer on SEN-11171 - FlyCamOne eco V2Pyroferurn:uuid:4f0de50d-9fb2-0927-1186-f5e935d3d6c02012-05-21T04:29:55-06:00<p>Nowhere can I find the type of sensor, is it CCD or CMOS?<p>I want a global shutted NOT rolling shutter, there are hundreds of cheap CMOS spy cams, the only reason for buying this is if it's CCD.</p><p>PLEASE tell me it's CCD...</p></p>
mux on SEN-11171 - FlyCamOne eco V2muxurn:uuid:5b45ce66-311b-4053-6ff3-e3365bd185a82012-05-19T19:56:42-06:00<p>It could be the FAT fs, it doesn't support files larger than 4GBs.</p>
Customer #23647 on SEN-11171 - FlyCamOne eco V2Customer #23647urn:uuid:31801b1d-1193-d867-5ba1-8a8d158b4d3a2012-05-13T20:26:43-06:00<p>I had the idea to use this as a squirrel camera on my fence, but the serial photos stop after 45 pictures. This occurs using the battery connector and the servo connector for power. Has anyone else had this problem?</p>
VonChurdhousen on SEN-11171 - FlyCamOne eco V2VonChurdhousenurn:uuid:ed012aac-1c9c-bbfb-f583-5407ac8d04e42012-05-12T00:05:49-06:00<p>I was successful in updating the drivers using an older pc running Windows XP. 7 wouldn't let me use unsigned drivers. Also had to reformat my microSD. Works great!</p>
Customer #44949 on SEN-11171 - FlyCamOne eco V2Customer #44949urn:uuid:08c4a5dc-d4af-222b-b227-48a74360f0e52012-05-11T16:43:34-06:00<p>Here are some notes for the EVO FlyCam2 in R/C applications.<p>FC2 has 3 modes: Video, Serial-Photo�which takes stills one at a time, and Single-Photo. Each mode is indicated by a different LED color and flashing pattern.</p><p>Fast flashing green LED means Single Photo mode is ready, and slow-flashing green means Single Photo mode is ready. The two remaining modes flip/unflip the picture 180 degrees. Point is, to get videos, you have to have a solid green led, then cycle switch or button less than 3 seconds to toggle video capture ON/Off.</p><p>At power-up, FC2 normally starts up in �Video� mode indicated by the LED showing solid green. If LED is not solid green, FC2 is in a mode other than �video� and you must change it, assuming you want to shoot videos. When the Transmitter�s (TX) switch or button is �on� (closed) MORE THAN 5 SECONDS the FC2 will SWITCH TO THE NEXT MODE.</p><p>If the receiver channel to which the FC2 is attached is controlled by a switch rather than a button, you must CYCLE THE TX�s SWITCH from from OFF to ON to OFF in no more than 3 seconds to BEGIN/END the mode�s processing, whether video or still. OR if a button controls the channel rather than a switch, you simply PUSH THE BUTTON to start and then push it again to stop the mode�s processing. Be sure to hold down the button no more than 3 seconds.</p><p>Prior to power-up, remember to turn video card switch to ON. Turn video capture switch/button on TX to OFF then turn TX ON. If solid green, video is ready; Otherwise, cycle to correct mode as explained above.</p><p>Hope this helps</p><p>DOZ</p></p>
CHaskins on SEN-11171 - FlyCamOne eco V2CHaskinsurn:uuid:f30049e9-dddd-6cee-4255-ac7adc9dd8112012-05-05T08:33:25-06:00<p>I tried five times, it would only record for just shy of two hours each time I tried it and max of 4gb, must be the size of the buffer onboard.</p>
relaxing on SEN-11171 - FlyCamOne eco V2relaxingurn:uuid:6d4968c6-6e51-5b14-7a09-53d39c5b96bc2012-05-05T07:52:37-06:00<p>Could be a 2gb limit?</p>
sub_lieutenant on SEN-11171 - FlyCamOne eco V2sub_lieutenanturn:uuid:9a676b92-52cf-0a25-c238-0199b2793c182012-04-26T19:13:31-06:00<p>Is the camera waterproof/watertight?</p>
CF on SEN-11171 - FlyCamOne eco V2CFurn:uuid:5703c375-74f1-48b5-c4e6-facf12a454472012-04-24T16:39:49-06:00<p>I have a question about the servo connector. The manual says this is for a button press on the transmitter. What signal is the camera expecting? Is it a 0 to 180 degree transition? or is it a simple on-off pulse?<p>Tried capturing serial images by using the arduino servo "sweep" example but I'm not getting consistent results. I assume I should get one picture per sweep, but I'm getting pictures at random times.</p><p>What gives?</p></p>
Pearce on SEN-11171 - FlyCamOne eco V2Pearceurn:uuid:af6304fd-5eab-bd33-7c35-8b3aa756510f2012-04-18T10:03:09-06:00<p>Using a 2Gb, I was able to get a little over 20 minutes.</p>
shortedneuron on SEN-11171 - FlyCamOne eco V2shortedneuronurn:uuid:c4e345fb-d060-260a-4c14-ecdd65f186412012-04-16T15:47:46-06:00<p>like previous comment, i notice your example footage is “unavailable” on Vimeo. I'd quite like to see that before buying one.</p>
MikeGrusin on SEN-11171 - FlyCamOne eco V2MikeGrusinurn:uuid:95415ede-f593-4b89-6218-1408012f34ce2012-04-12T14:32:48-06:00<p>No streaming, it records video and audio to the uSD card for later playback.</p>
ygr on SEN-11171 - FlyCamOne eco V2ygrurn:uuid:a4f2ea63-feb2-fcb2-7e9e-677478786e8d2012-04-12T06:43:53-06:00<p>I don't get it from the description nor the video. Is this capable of live streaming the video to pc/mobile/something?
Thanks!</p>
CHaskins on SEN-11171 - FlyCamOne eco V2CHaskinsurn:uuid:f4391177-fe38-3989-80d7-cd4133b8d3452012-04-10T18:38:09-06:00<p>I got 1hr 49mins 3secs using 4.0gb on an 8gb microsd. almost two hours and only half the card was used. Don't know why it stopped battery might have died I'll have to check.</p>
meetar on SEN-11171 - FlyCamOne eco V2meetarurn:uuid:0b3cdecc-f951-ec75-16e0-57551e0e8f0e2012-04-04T09:38:30-06:00<p>Do you know anything about the timing of the "serial images"? Is that timelapse? Can you set the delay between the images?<p>Thanks!</p><p>(btw, your example footage is "unavailable" on Vimeo.)</p></p>
Allan4 on SEN-11171 - FlyCamOne eco V2Allan4urn:uuid:782877dd-d218-dd62-9d24-813990c80bc02012-04-03T18:33:49-06:00<p>Uses the standard rc servo protocol,PWM. you can control it using the standard arduino servo library.</p>
ChuckM on SEN-11171 - FlyCamOne eco V2ChuckMurn:uuid:f8d5c741-6a6e-10dd-6d0a-1cc8ac16aa472012-04-01T14:21:26-06:00<p>As cool as this is from a project perspective. What is even cooler IMO is that it appears to be plug and play with a standard R/C receiver.</p>
Customer #87485 on SEN-11171 - FlyCamOne eco V2Customer #87485urn:uuid:af629b9a-0b9d-5a24-edaa-777a17de38702012-04-01T13:08:57-06:00<p>Is it possible to use this as a webcam so it could be attached to a beaglebone and used with opencv?</p>
Customer #283857 on SEN-11171 - FlyCamOne eco V2Customer #283857urn:uuid:0a87bfb8-1964-3658-230f-db90801fd0132012-04-01T12:36:08-06:00<p>how to interface with arduino?</p>
liutas4x4 on SEN-11171 - FlyCamOne eco V2liutas4x4urn:uuid:c5219c28-7238-c0f8-9d1c-1275e041783f2012-04-01T11:38:43-06:00<p>thank you!</p>
Young Maker on SEN-11171 - FlyCamOne eco V2Young Makerurn:uuid:0f637033-df30-cc78-4c19-ef5c8889c3c42012-04-01T09:53:37-06:00<p>its probably a more raw encoding. To make the file smaller, put the SD in a computer and use a video editing program to export it to a smaller file type, such as MPEG or mp4.</p>
patrickmorrison on SEN-11171 - FlyCamOne eco V2patrickmorrisonurn:uuid:8a80276a-f253-ba01-f352-d91b0f28bf122012-04-01T03:33:03-06:00<p>Are you sure usually 1 hour of high quality video is 1gb</p>
Customer #268820 on SEN-11171 - FlyCamOne eco V2Customer #268820urn:uuid:38122370-bc32-f7b1-2dbb-22382dbc92342012-04-01T02:29:30-06:00<p>1gb = 10 min recording</p>
CrazyCreator on SEN-11171 - FlyCamOne eco V2CrazyCreatorurn:uuid:41f326d5-aac7-81a7-3898-70384b018a402012-03-31T19:16:16-06:00<p>What is the pinout of the 3-pin connector? Also, what kind of signal does it use to control the start/stop?</p>
SomeGuy123 on SEN-11171 - FlyCamOne eco V2SomeGuy123urn:uuid:28550639-9c0b-bd85-ae34-af43ceb5d2fb2012-03-31T18:28:48-06:00<p>Someone should make a microSD to SD converter that has a form similar to <a href="http://www.sparkfun.com/products/9237" rel="nofollow">this board</a>.</p>
Sam_Bamboo on SEN-11171 - FlyCamOne eco V2Sam_Bamboourn:uuid:ecd44a82-7529-eeaf-5829-b072c1ecb7b72012-03-30T21:46:57-06:00<p>So is it black or white? :D</p>
Mecharius on SEN-11171 - FlyCamOne eco V2Mechariusurn:uuid:ecb23b88-92f5-90ab-384c-a79dc18837e42012-03-30T18:26:48-06:00<p>Or to a computer? Live video feed would be amazing</p>
joshl on SEN-11171 - FlyCamOne eco V2joshlurn:uuid:f3e88e07-f714-f91e-11ad-9209a615f1652012-03-30T15:37:57-06:00<p>agreed. we need to know total recording time.</p>
emihackr97 on SEN-11171 - FlyCamOne eco V2emihackr97urn:uuid:154eba82-7857-30e8-295a-3f15e53bca192012-03-30T14:09:05-06:00<p>Do you have something to actually stream Live video back to an iPhone or something?</p>
liutas4x4 on SEN-11171 - FlyCamOne eco V2liutas4x4urn:uuid:21ef621d-4d1e-4e50-8f34-9a7c899b58e22012-03-30T13:21:17-06:00<p>Total time, possible to record on 8Gb?</p>
JohnK-EvilMinion on SEN-11171 - FlyCamOne eco V2JohnK-EvilMinionurn:uuid:68fe80ca-8f3a-5fdc-f1cb-839dc31757d42012-03-30T13:13:22-06:00<p>What is the max recoding time for 2GB and 8GB micro SD cards?</p>
Dougie on SEN-11171 - FlyCamOne eco V2Dougieurn:uuid:f145176e-01c0-9eee-033c-7177979409e72012-03-30T12:39:00-06:00<p>The buffering issue mentioned in the video suggests that the eyefi won't get written to until you stop the recording. unless you remotely control recording there's kinda no point.</p>
Spiku on SEN-11171 - FlyCamOne eco V2Spikuurn:uuid:708560c1-6527-f150-3c87-e2075e9d073c2012-03-30T10:39:31-06:00<p>Since the pin-outs are (basically) the same, could you wire a regular SD slot in place of the MicroSD slot?</p>
aaronbear on SEN-11171 - FlyCamOne eco V2aaronbearurn:uuid:ba69bba3-df9d-959c-7162-462e3d21d6be2012-03-30T10:36:42-06:00<p>Is there a UART or other output to hook this bad boy up to a micro controller or xbee? Maybe hidden under that plastic wrapper? I'm surprised you guys didn't rip the wrapper off for your new product post.</p>
RobertC. on SEN-11171 - FlyCamOne eco V2RobertC.urn:uuid:a05df370-0cdb-074a-e8ca-95583f8b00572012-03-30T09:53:58-06:00<p>It's MJPG, but apparently there's a firmware update in the works that does h.264. file is an AVI.</p>
bbotany on SEN-11171 - FlyCamOne eco V2bbotanyurn:uuid:7f927124-d250-d28b-6411-e65392272f9e2012-03-30T09:02:47-06:00<p>What video encoding does this record to? I read through the linked materials, but didn't see the format mentioned, just the resolution&fps.</p>
St.Eligius on SEN-11171 - FlyCamOne eco V2St.Eligiusurn:uuid:fdd06561-689d-1664-9774-60ae9b9927e62012-03-30T06:21:19-06:00<p>Too bad the thing doesn't seem to have ntsc/pal outs.</p>
Robdrech on SEN-11171 - FlyCamOne eco V2Robdrechurn:uuid:2920ee6b-c1ba-1019-87ca-ba611b158c442012-03-29T20:58:47-06:00<p>Too bad that it's a micro sd and not standard SD... Then you could stuff a Eye-fi there and be styling!!</p>
MostThingsWeb on SEN-11171 - FlyCamOne eco V2MostThingsWeburn:uuid:acc0f1bf-f02c-142d-1612-9edbfd64cfdc2012-03-29T18:37:30-06:00<p>Not a problem. Thank's for fixing that. Quick question also: Would the servo in the Related Products fit the tilt-mount, or does the camera already have a motor built in? Alternatively, do I just have to preset the swivel manually?</p>
Nate on SEN-11171 - FlyCamOne eco V2Nateurn:uuid:0890c8ac-6b19-b140-a8bc-97dc149ce6912012-03-29T18:36:24-06:00<p>No problem! Sorry for the omission. I updated description as well.</p>
MostThingsWeb on SEN-11171 - FlyCamOne eco V2MostThingsWeburn:uuid:7b6a011a-94a2-6fb6-59f3-1ebbb772f7c72012-03-29T18:26:53-06:00<p>*Adds to wishlist* Sweet, thanks!</p>
Nate on SEN-11171 - FlyCamOne eco V2Nateurn:uuid:92c13a74-dce9-38d3-5d10-8defab18ed462012-03-29T18:25:44-06:00<p>Full color.</p>
MostThingsWeb on SEN-11171 - FlyCamOne eco V2MostThingsWeburn:uuid:004c88b2-6ac5-425b-00ad-2dc9d6fb0f2e2012-03-29T17:46:51-06:00<p>Is it color or black-and-white? The manual doesn't say.</p>