SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T06:25:56-06:00SparkFun ElectronicsLeandro Lima on TOL-11298 - 4 Pin Molex Connector - PigtailLeandro Limaurn:uuid:8af7fcdf-1bf4-f3cc-c47b-5a497a64be932014-08-05T12:35:46-06:00<p>Is there a female connector too?</p>
Customer #462137 on TOL-11298 - 4 Pin Molex Connector - PigtailCustomer #462137urn:uuid:ee9d13b0-2658-361f-e2e5-076fcc633c6b2013-08-15T17:19:40-06:00<p>We purchased several of these pigtails and the gauge was fairly small looks like 22ga according to the wire stripper. The ends were tinned which is nice.<p>The crimp connections didn't seem very solid, wires were able to be pulled out of the crimped terminals without much trouble. This was a convenience for me but under normal cases I wouldn't want to be able to do that without cutting or breaking the wire itself.</p></p>
Ed Hartnett on TOL-11298 - 4 Pin Molex Connector - PigtailEd Hartnetturn:uuid:48d03326-17ba-0f6d-c3b4-e717c591c2d22012-12-02T11:25:33-07:00<p>No, it doesn't, but I wish it did, or at least there was a link to the matching female part, I can't find it...</p>
MostThingsWeb on TOL-11298 - 4 Pin Molex Connector - PigtailMostThingsWeburn:uuid:805eaa92-878c-7de9-7c5e-e9bef6dc88fc2012-08-10T13:14:22-06:00<p>No, I don't think so.</p>
Customer #339550 on TOL-11298 - 4 Pin Molex Connector - PigtailCustomer #339550urn:uuid:cd6e94b5-f702-2010-84f4-1da75a3964212012-07-20T08:34:05-06:00<p>Does the 4 pin Molex Connector - Pigtail TOL-11298, witch is showing only the male connector, does it comes with the female part ??</p>
dwild on TOL-11298 - 4 Pin Molex Connector - Pigtaildwildurn:uuid:7a54c907-9383-c078-e233-28ada3da5f242012-07-13T22:15:13-06:00<p>What is the gauge of these wires?</p>