SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T17:22:50-06:00SparkFun ElectronicsNikos Monios on COM-11311 - Toggle Switch and Cover - Illuminated (Green)Nikos Moniosurn:uuid:5353f0d7-f563-1a62-6596-74dfea1ef22e2014-09-24T16:10:45-06:00<p>I would like to use a switch for the power supply circuit on my quadcopter.<p>I use a LiPo battery, 11.1 Volts, 3300 mAh and the continuous current of the ESC is 20 A.</p><p>Will this switch do the job?</p></p>
lawnmowerlatte on COM-11311 - Toggle Switch and Cover - Illuminated (Green)lawnmowerlatteurn:uuid:a6a44fce-f50e-0029-601d-5e2ff71c98842014-08-07T22:52:14-06:00<p>How is the illumination controlled? Is it always on or is it only on when the switch is on?<p>Edit: Nevermind, I see there's a third input. <a href="http://youtu.be/mjUKK2gzenw?t=1m49s" rel="nofollow">Video here</a></p></p>
Customer #513342 on COM-11311 - Toggle Switch and Cover - Illuminated (Green)Customer #513342urn:uuid:72c8e124-d35c-c5fd-1a9d-4fc41024d7132014-01-25T19:37:22-07:00<p>Hi I want to put these in my 98 jeep cherokee sport, I’m thinking about switching out my rear defrost, rear wipers, and my fog lights for these switches. I need more help trying to figure out if they will fit or if they won’t, so can anyone help me, also I need to know how I to wire them up, if I get them?</p>
Customer #252418 on COM-11311 - Toggle Switch and Cover - Illuminated (Green)Customer #252418urn:uuid:db72312f-8de8-b5fa-4f39-f4dc05c1e4442013-06-27T12:59:46-06:00<p>Can the cover protect the switch in the ON position or does closing the cover automatically switch it to OFF? I realize you could wire it the other way, but then would the cover need to be slightly raised to leave it in the OFF position? Thanks!</p>
rsp on COM-11311 - Toggle Switch and Cover - Illuminated (Green)rspurn:uuid:a4939675-fa25-9b0c-b854-bf0e445fee492012-08-04T09:59:24-06:00<p>These switches not weather proof nor explosion proof, and they're very likely not safe for use with AC line voltages.<p>Also, the connectors are all 1/4" fastons. The overall dimensions (with cover closed) are 0.675" wide, 2" high, 2.675" deep. The panel mounting stud is 1/2" long (can be used with panels up to 1/4" thick).</p></p>
Customer #273244 on COM-11311 - Toggle Switch and Cover - Illuminated (Green)Customer #273244urn:uuid:43bc5d0c-3c61-0393-c892-09eee3b8970a2012-07-03T15:18:34-06:00<p>Is this weather-proof?</p>
Noobulus on COM-11311 - Toggle Switch and Cover - Illuminated (Green)Noobulusurn:uuid:ad8265c2-7ee0-2349-6b9b-b3a79ccdfe2e2012-06-19T20:14:43-06:00<p>The quarter is a spy!</p>
RobertC. on COM-11311 - Toggle Switch and Cover - Illuminated (Green)RobertC.urn:uuid:2f935bf5-a3c2-82cf-44d6-fb3babc202ec2012-06-15T09:43:29-06:00<p>it's never been circulated, straight from the mint.</p>
disabelle on COM-11311 - Toggle Switch and Cover - Illuminated (Green)disabelleurn:uuid:7f95a8c8-6f05-07cd-e76e-76eabf6848052012-06-14T23:55:08-06:00<p>i looks like the quarter is a fake.</p>