SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T23:35:24-06:00SparkFun ElectronicsLordVilla on DEV-11361 - Arduino Ethernet with PoELordVillaurn:uuid:2cc5e775-0f19-e5d5-df6c-fa5d01c6ff7a2015-04-20T10:00:27-06:00<p>Why this product have been retired from the catalog? any reason in particular?</p>
Customer #33900 on DEV-11361 - Arduino Ethernet with PoECustomer #33900urn:uuid:fcfde948-8655-be1e-d696-d8d68ca217652014-03-28T18:50:32-06:00<p>Anyone know if you can use ICSP header on this one to talk to another device via SPI?
With the Ethernet shield version it uses the ICSP header so it's a no-go, wondering if it would work on this one.</p>
Toni_K on DEV-11361 - Arduino Ethernet with PoEToni_Kurn:uuid:e1c56586-a242-ebe7-3a79-ff31fc4740d12013-10-30T10:28:07-06:00<p>Email techsupport@sparkfun.com. They may have heard of this error, or might have some additional insight into this for you. Sorry to hear about the difficulties with your project!</p>
Customer #43547 on DEV-11361 - Arduino Ethernet with PoECustomer #43547urn:uuid:4b922d6d-001b-aeff-f001-c62260c6e4032013-10-29T16:46:30-06:00<p>I bought a bunch of these for a home automation project. It seems like they are all defective, or I'm doing something horribly wrong... Basically, one of them heats up so bad that I'm confident it might catch fire or burn out. The other units all exhibit the same strange behavior. They work fine for about 6-18 hours, and then they stop. All I use them for is to send temperature sensor readings every 60 seconds, but after less than a day of usage, they all stop transmitting. The units remain on, but nothing happens. I've tested it with 3 different POE switches, including an enterprise 24 port switch and the results are always the same. There are no firewalls in place. If I unplug them and plug them back in, they all work just fine and then turn off after about 6-18 hours. Just wanted to post this in case someone else experienced the same problem or knows how to fix it.</p>
IrvinPoncePerez on DEV-11361 - Arduino Ethernet with PoEIrvinPoncePerezurn:uuid:e0007a0c-1343-aaf9-2e92-be7508222b112013-10-15T10:34:10-06:00<p>Hello I have the RFID Evaluation Shield - 13.56MHz and I want to know if I can use the the Arduino Ethernet with module PoE and RFID Evaluation Shield I can see that the module PoE is big?</p>
M-Short on DEV-11361 - Arduino Ethernet with PoEM-Shorturn:uuid:12aba916-60b4-de53-c747-b832f927615b2013-02-11T14:10:19-07:00<p>Check the datasheet for the POE module listed on Arduino's page. It is indeed 802.3af compliant.</p>
liger on DEV-11361 - Arduino Ethernet with PoEligerurn:uuid:50666d8d-c926-f867-e727-91505d74d92d2012-10-12T18:46:11-06:00<p>is it really necessary to have ftdi breakout for this? I tought it would upload the program directly over Ethernet?</p>
71784 on DEV-11361 - Arduino Ethernet with PoE71784urn:uuid:92f37d81-d972-4429-5720-b6b01ff104b12012-08-31T19:44:20-06:00<p>Arduino Italy said they incorporated version 4.4 firmware starting October 2011 on these boards.
Are these boards in Sparkfun inventory pretty new?</p>
TechShopRDU on DEV-11361 - Arduino Ethernet with PoETechShopRDUurn:uuid:c21851a4-798c-96f7-f0be-4a4e18dc51e02012-08-30T22:45:11-06:00<p>Just to confirm: This is IEEE 802.3af compliant, right? Unlike some other products SparkFun has called "PoE" in the past? (Like https://www.sparkfun.com/products/10864 )</p>
M-Short on DEV-11361 - Arduino Ethernet with PoEM-Shorturn:uuid:36b8f5e5-a655-a8f2-26c6-f0b2767559182012-08-06T09:28:49-06:00<p>When you work in a rocket test facility everything is rocket science!</p>
Jamster on DEV-11361 - Arduino Ethernet with PoEJamsterurn:uuid:fcdfe9b6-0cc4-5f51-638d-56c883c50db72012-08-04T12:51:41-06:00<p>Come on! LCD and a switch?!? That's not exactly Rocket Science is it?!? :P</p>
bazookazuz on DEV-11361 - Arduino Ethernet with PoEbazookazuzurn:uuid:44f40ab3-3bbc-4ba4-3d09-2483f800785e2012-08-03T09:40:01-06:00<p>this is a great product. you plug in one wire and you get everything you need. I am a programmer for a rocket test facility. i bought a pile of these, added a switch & LCD and presto chango! ethernet abort buttons! rocket scientist approved!</p>