SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T02:43:31-06:00SparkFun ElectronicsCustomer #797661 on COM-11372 - LED - Basic Blue 5mmCustomer #797661urn:uuid:f22283a0-bbe6-363f-5791-8445efce55462018-03-15T15:12:32-06:00<p>How well do these work as a replacement for the 3V6 zeners in a v-usb project operating at 5 volts? Current is 25mA assuming 3.4V Vf, btw, due to 68 ohm resistors. (3V6 zeners over 3V3 due to the I/V curve placing 3.3V at 100s of mA on a 3V3 zener, iirc)</p>
ferranpce on COM-11372 - LED - Basic Blue 5mmferranpceurn:uuid:fa2a3aab-4485-b3df-7aa8-53a1a307bc5a2014-08-20T08:29:45-06:00<p>What is the wavelength for this one?<p>Also, I measured 2.8V forward drop.</p></p>
Sparky91381 on COM-11372 - LED - Basic Blue 5mmSparky91381urn:uuid:3bb53eb4-e3cc-51bb-8fea-f909f20edc902013-12-04T14:20:48-07:00<p>hard to find blue diffused leds so when i saw them i jumped for joy - these things are bright and impressive - just what i was looking for</p>