SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-29T01:40:20-06:00SparkFun ElectronicsCustomer #564778 on RTL-11422 - EL Wire - Red RetailCustomer #564778urn:uuid:80737480-bd7c-a348-96ef-ad735f5ac67f2014-06-19T14:07:38-06:00<p>Question 1. If I put 2 or n , ELwires connected in series , how I calculate the mA ? there is nothing at the pdf for this
I want to connect 2m or 3m and make it 4 or 10 meters , just like you do at the datasheet. Put it on an inverter with a MOC and triac, and then control it with arduino. I see the datasheet of the inverters you have for this and the EL Escudo , so 8 EL is 1,5A?<p>So I want help with the limits to make it safe and not make it hot or ... anything</p><ol start="2">
<li>how I can dimmer this? I search some solution for it with pwm at the inverter input with a transistor</li>
</ol></p>