SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T16:28:33-06:00SparkFun ElectronicsCustomer #625664 on WRL-11786 - Bluetooth SMD Module - RN-41Customer #625664urn:uuid:6f9e64fa-dc1f-5cb8-c817-f7ef3fe34cfb2014-12-05T13:16:48-07:00<p>quick question: is SM,6 supported on this firmware? i can't seem to find any reference in the revision history...
tia</p>
Customer #542563 on WRL-11786 - Bluetooth SMD Module - RN-41Customer #542563urn:uuid:ed88a390-f3ca-21df-512d-71e9d6c689642014-04-06T12:00:41-06:00<p>How is this module better than HC05? Just wondering, I'm using HC05 only as a slave device, what do I gain switching to this?</p>
Customer #450621 on WRL-11786 - Bluetooth SMD Module - RN-41Customer #450621urn:uuid:2f9ff035-b2aa-480d-c7e0-52e746efced02013-08-11T09:56:38-06:00<p>i got it working, sweet, and my code is there too. (under RN41)
http://www.fixkick.com/ELM327/taurus-sim/hacked.html#MPG</p>
Customer #450621 on WRL-11786 - Bluetooth SMD Module - RN-41Customer #450621urn:uuid:89ef77ac-f29c-a647-98fe-79dc8a1632902013-07-24T11:37:55-06:00<p>mouser is a full wholesale distr. and sells by quantity discounts, as do most wholesalers.<br>
the data sheet is clear see second bullet !, it states. "Backwards-compatible with Bluetooth version 2.0, 1.2, and 1.1 "
read the real data sheets and the real full PDF, this module is far better than any HC05 sold, and 1000 time better docs and support.
I wish now that i didn't waste my time on CSR parts (HC05)<p>using three?, of these. the pdf above shows. only 1 master talking to 1 slave. RTM.</p><p>my wish,why not make sell this module mounted, to a base board, with header pins so we can connect to it.
those castellated pins are very hard to use. unless doing a custom PCB SMT layout.
If I missed a base board, please post that.</p></p>
dnear1 on WRL-11786 - Bluetooth SMD Module - RN-41dnear1urn:uuid:a5b8e4b9-fcf0-eb9f-48f1-ac705cc0595a2013-07-21T19:11:40-06:00<p>I was thinking to use three of these units. One as a base and two as remotes. Both remotes would need to connect simultaneously with the base (Data rate will be really low and intermittent, but random). Is that possible with these Bluetooth modules? Or do I have to use Zigbee?</p>
Customer #229304 on WRL-11786 - Bluetooth SMD Module - RN-41Customer #229304urn:uuid:5b95bddc-16b5-3037-55c9-1c58bbf66e3c2013-06-17T06:00:34-06:00<p>Why no quantity price breaks? :(</p>
thebrit on WRL-11786 - Bluetooth SMD Module - RN-41thebriturn:uuid:d479176c-d9a7-e6e4-fe5a-78322dab19702013-05-28T13:44:09-06:00<p>BTW - This is BT2.1 with EDR, not BT2.0 as listed in the bullets above.</p>
thebrit on WRL-11786 - Bluetooth SMD Module - RN-41thebriturn:uuid:a533f108-df09-da14-10f0-c598f3b64f272013-05-28T13:42:57-06:00<p>Cool - a long range (100m) version of the RN42</p>