SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T18:42:44-06:00SparkFun ElectronicsToni_K on COM-11903 - ELastoLite Panel - 5x3 inches - Blue-GreenToni_Kurn:uuid:4af5cf46-a596-e4c9-90c7-fa2692df6cb02015-01-08T09:45:42-07:00<p>Supposedly, yes. You'd have to be very, very careful to not end up shorting the two layers internally (and ruining the panel). However, then you can't use the flexibility feature of this, as that would likely lead to the cut ends shorting.</p>
Customer #529272 on COM-11903 - ELastoLite Panel - 5x3 inches - Blue-GreenCustomer #529272urn:uuid:b70b6c7e-1e4e-22ca-6895-e2f4dc6dfca82015-01-07T17:54:13-07:00<p>Aside from the waterproofing can these be cut without killing the panel.</p>
Customer #613005 on COM-11903 - ELastoLite Panel - 5x3 inches - Blue-GreenCustomer #613005urn:uuid:b0eea903-c144-d2dd-d379-e0ae016e65a22014-11-02T16:13:15-07:00<p>can the Elastolite panel be heat pressed directly to fabric ?</p>
Toni_K on COM-11903 - ELastoLite Panel - 5x3 inches - Blue-GreenToni_Kurn:uuid:c44fba92-21f1-4e53-19dd-679daa2ef2bd2014-05-14T13:07:52-06:00<p>It ruins the waterproofing on the panel, which is one of the biggest features of this material.</p>
Customer #137238 on COM-11903 - ELastoLite Panel - 5x3 inches - Blue-GreenCustomer #137238urn:uuid:ef5479d4-e131-9be3-0f05-2d54499dd2362014-05-14T11:29:38-06:00<p>I was wondering the same... Why can't you cut this?? thanks</p>
Customer #384912 on COM-11903 - ELastoLite Panel - 5x3 inches - Blue-GreenCustomer #384912urn:uuid:f2a8253f-c405-313a-d840-13f74f25367a2014-02-10T18:47:33-07:00<p>Why can't this be cut?</p>